Part Number: LMR38010-Q1 Other Parts Discussed in Thread: LMR38015-Q1 Hi team
Could you please hlep share LMR38010-Q1 EMI test report? It should include the test setup, circuits including the filter design, test condition and CE RE test result per CISPR…
Part Number: LMR38010-Q1 Hi experts,
My customer is asking in <LMR38010-Q1 Functional Safety FIT Rate, FMD and Pin FMA> document, there is not description about short any two pins in FMD. Please help to support how to calcuate the FIT? Is that okay…
Part Number: LMR38010 Tool/software:
Given that the minimum value for the HS switch limit is 1.3 A and the low side switch limit is 0.9 A (FOR LMR38010), if we have a load current of 1A and a total current change ( ΔI) of 0.4 A, it will always exceed…
Part Number: LMR38010-Q1 Hi team,
I have a question regarding the threshold voltage of enable function.
VEN-H and VEN-L overlap each other, for example, VEN-H = 1.1V and VEN-L = 1.22V. Is there hysteresis on these threshold voltage?
Best regards…
Part Number: LMR38010 Tool/software: I am using LMR38010 in inverted buck boost topology to generate a -70V output from a 5V input. To my understanding this is equivalent to a 75V input and 70V output, and I use this voltage range as the input parameters…
Part Number: LMR38010-Q1 Hi Team,
we are looking for a LTSPICE usable model. We already have send the customer our unencrypted model, but it seems like they are not working in LTSPICE. Do you have any suggestions to convert those in order to make…
Part Number: LMR38010-Q1 Other Parts Discussed in Thread: LMR38010 , LMR38020 Tool/software: Hi team,
Could you please provide efficiency data of LMR38010-Q1 at 48V input and 2.2MHz 12V/1mA output?
Customer is concern about light load current consumption…
Part Number: LMR38010 Hello expert,
As talked, there is no calculator for LMR38010 but we have WEBENCH simulation result like output ripple. Do we have a chance to have the calculator for LMR38010 which includes output ripple? Customer has output ripple…
Part Number: LMR38010 Tool/software: Hello. There are two recommended layouts for DDA package in the datasheet for LMR38010FSDDAR part. They have different exposed pad sizes. Which one should be followed? DDA0008B from 2016 or DDA (R-PDSO-G8) from 2012…
Part Number: LMR38010 Other Parts Discussed in Thread: , LMR38020 , LMR38020EVM HI~
If the surrounding environment is the same (layout, load, etc...)
1. If only LMR38010 frequency and L (200MHZ ~ 2.2 MHz), are EMI characteristics the same?
2. Are…