Part Number: LMR38010-Q1 Other Parts Discussed in Thread: LMR38020-Q1 , regarding the chip LMR38010-Q1/LMR38020-Q1, could you provide me some power loss calculation sheet for the chip?
Part Number: LMR38010-Q1 Other Parts Discussed in Thread: LMR38010 I am using the LMR38010 as an inverting buck-boost regulator to convert 24V to -7V. Should the EP pad be connected to the GND pin which becomes the negative output of the converter as…
Part Number: LMR38010 Tool/software: Hi All
The output capacitor table for LMR38010 is shown above. For calculations involving a voltage conversion from 24V to 12 V at a frequency of 1000kHz , with an output current of 1A, a current ripple ration…
Part Number: LMR38010 Dear e2e Support,
Can we share our spec for the Vref tolerances, in PFM mode?
Is it out of spec to get a Vref measurement above 1.04V, in this mode?
Regards,
Part Number: LMR38010 Other Parts Discussed in Thread: TPS40055 Hi,
I have a question concerning the FPWM of the LMR38010FSDDAR.
Take a basic circuit with 48V input and 9V output.
In my application it might be that the output is pulled higher than…
Part Number: LMR38010 Other Parts Discussed in Thread: LMR38020EVM HI~
The link below says, “GND should not be placed under the INDUCTOR.”
https://techweb.rohm.com/product/power-ic/dcdc/dcdc-design/3254/
However, DATASHEET 11.2 LAYOUT EXAMPLE has…
Part Number: LMR38010 Hi Expert,
I want to check if LMR38010 have function to switch PWM or FPWM automatically?
Or device only have one mode and need to choose different part number?
Thank you.
Part Number: LM5163 Other Parts Discussed in Thread: LMR38010
Hello,
I was wondering:
what is the behaviour of LM5163 and LMR38010 SW pin when some current is injected on Vout (from 0mA up to 50mA), with Vout=0 i.e. when Vout rail is pulled up by…
Part Number: LMR38010 Other Parts Discussed in Thread: LM5163 Hi team,
Does LM5163 can be directly replaced with LMR38010 without any hardware change? I noticed that the EN &VIN pins are a little different.
Part Number: LMR38010
Hi all
I would like to know Spread Spectrum function at light load.
The device enters PFM mode at light load.
I understand switching frequency is lower in PFM mode.
・Is Spread Spectrum functioning in PFM mode?
…