Part Number: LMR38020-Q1 Hi Team,
I was looking for 48V to 12V conversion solution using LMR38020-Q1. If I would get a ready schematics and PCB files, it will easy for me to implement.
Thanks in advance.
Shubham
Part Number: LMR38020-Q1 Hi team,
I am helping customer to do technical review on this part for a 24V automotive lighting application.
Could you share the following information inside LMR38020-Q1?
Dead time control logic and range
2. Switch…
Part Number: LMR38020-Q1 My customer, YURA is looking for alternate solution of ADI, LT80602.
norminal required current is <1A, normally 500mA. customer need high effeciency at light load.
LMR38020SQDDARQ1(PFM) is recommended because it has higher…
Part Number: LMR38020-Q1 Tool/software: Hi team,
My customer has been considering adding the snubber circuit(R + C) on the SW pin to prevent EMI. Is there recommended value of snubber circuit?
Best regards,
Shunsuke Yamamoto
Part Number: LMR38020-Q1 Tool/software: Hi team,
It seems there are two patterns of package information, and the size of thermal pad is different. Which one is correct?
Best regards,
Shunsuke Yamamoto
Part Number: LMR38020-Q1 Other Parts Discussed in Thread: LMR33620-Q1 , LMR36520 , LMR33620 , LM46002-Q1 Tool/software: Hi expert,
My customer (CosMX) is looking for a suitable device which functional block diagram is closed to LMR33620-Q1, and meet…
Part Number: LMR38020-Q1 Tool/software: Hello Team
i have done LMR38020-Q1 transient simulation and it worked fine. While i changing the simulation to files to other location or giving save project as option, an error is coming like as below. Can…
Part Number: LMR38020-Q1 Hi Team,
We found encrypted model at LMR38020-Q1 datasheet page. Please provide unencrypted SPICE model for LMR38020-Q1.
Here is the NDA number b/w HCL Tech and TI.
2017-11-08-00470M
Need urgently. Would you please provide…
Part Number: LMR38020-Q1 I had downloaded the spice model LMR38020-Q1 for LTspice simulation. But I am able to run the circuit because of encrypted library file. Kindly provide the unerupted version.