Part Number: LMR38025-Q1 Other Parts Discussed in Thread: LMR38025 Tool/software: Hi! In my design, I am using the LMR38025SQDRRRQ1, and the VIN has a maximum of 60V. My design needs to comply with IEC 62841 / IEC 60730 PCB Routing and Creepage Requirements…
Part Number: LMR38025-Q1 Other Parts Discussed in Thread: LMR38025 , LMR38020EVM Tool/software: Hi,
I’m currently working on designing DC/DC buck converter to step down 24 V input voltage to 15 V.
Simulating transient response I get great results…
Part Number: LMR38025-Q1 Tool/software: hello i am looking for packaging information for the wson-12 package which has the ti package code drr looking at the packaging information page all i could find was just a generic package view but no dimensional…
Part Number: LMR38025-Q1 Tool/software: We are using LMR38025-Q1.
The no-load current is very high, i.e., 10 mA. Below are the key values of components
Input Voltage: 24 V
Switching frequency = 400 kHz
Inductor L1 = 15 uH
R FBT = 50K
R FBB = 10K
RT =64…
Part Number: LMR38025-Q1 The datasheet for the LMR38025-Q1 never says how to handle the FB pin for the fixed voltage versions. It says not to leave it floating or connect it to GND so, do I just run it straight to Vout? I am using the LMR38025S5QDRRRQ1…
Part Number: LMR38025-Q1 Hello TI support: I need the weight information for the LMR38025-Q1, I can not find it in the datasheet, please help to provide, thanks a lot!
Part Number: LMR38025-Q1 Other Parts Discussed in Thread: LMR38025 Looking at a secondary power input path for our design which would feed the same node as the output of the LMR38025 buck. In essence, this would raise Vout of the LMR above Vin
Can we…
Part Number: LMR38025-Q1 Other Parts Discussed in Thread: LMR38025 Currently we are working on Synchronous buck converter (Integrated Switch)
LMR38025-Q1 in Web bench Design for below parameter,
Input Voltage - 36V to 80V
Output voltage - 12V
Output Current…