Part Number: LMR43610 Tool/software: Hello, I have implemented a voltage regulator that converts a voltage ranging from 4V to 36V to a fixed voltage of 5V based on LMR43610R3RPER. The maximum current delivered by the regulator is 1.2A. Below is the schematic…
Part Number: LMR43610 Tool/software: Hi support team, I am looking for a device that can achieve the following specifications.
VIN: 3.5V~7.2V VOUT: -10V IOUT: 0.3mA Forced PWM
Is it possible to achieve this with the LMR43610MB3RPER inverting buck-boost? …
Hello,
Since we have not heard from you in a while, I am going to close this thread. You can re-open this thread by replying or create a new thread.
Best regards,
Ridge
Part Number: LMR43610 Tool/software: Hi,
Question 1: The input voltage of LMR43610 is 15V, the output voltage is 1.8V, and the load current is about 100mA. What is the approximate efficiency? Question 2: The input voltage of LMR43610 is 15V, the output…
Part Number: LMR43610-Q1 Tool/software: Hello experts,
Please allow me to check the current consumption of the LMR43610-Q1 at light loads.
Please let me know the current consumption at 2 mA output and 60 uA output.
The conditions are in Auto mode and…
Hello,
Since we have not heard from you in a while I will be closing this thread. If you have more questions, you can re-open this thread by replying or create a new thread.
Best regards,
Ridge
Part Number: LMR43610-Q1 Tool/software: Hi Application Team:
My customer need the both LMR43610MSC5RPERQ1 and LMR43610MSC3RPERQ1 Top marking detail naming, could you please give us the definition for both PN like as below ?
thank you
Part Number: LMR43610-Q1 Tool/software: Hi team,
From our recommendation, it looks that some settings don't fulfill the eq(6) requirement. This table means within ~500Ohm is OK?
Customer wants 8.5V output and plan to set Rfbt = 84.5kOhm, Rfbb =…
Part Number: LMR43610-Q1 Tool/software: Hello experts,
What is the power conversion efficiency of the LMR43610-Q1 at light loads?
We have the possibility of 60uA output, and we would like to share information on the power conversion efficiency curve…
Part Number: LMR43610-Q1 I would like to proceed with the circuit design using LMR43610MSC3RPERQ1 as follows.
VIN:12V VOUT: 1.8V IOUT: 1A
According to the datasheet, we are trying to combine R_FBT and R_FBB as follows. R_FBT: 17.8K_1% R_FBB: 22.1K_1%
Please…