Part Number: LMR43610 Tool/software: Hello TI Team,
We are using LMR43610 in one of our projects, can someone from TI team please verify the schematics of it and let us know if some changes are required.
Thanks & regards
Part Number: LMR51440-CALC Other Parts Discussed in Thread: LMR43610 I intend to perform DCDC circuit analysis using the SIMPLIS tool.
I would like to request the sharing of the SIMPLIS library for the LMR43610 component.
Part Number: LMR43610-Q1
Hi Team,
Could you help provdie Stability simulation for customer's design? Schematic will add later.
I tried to use Webench, but it showed not support, and the same for LMR43610-Q1
Thank you!
Marc
Part Number: LMR43610-Q1 Tool/software: I have a question about using the LMR43610-Q1 and the WEBENCH Power Designer.
My goal is to create a 3.3V/1A output, but the most available part for me is the LMR43610MSC5RPERQ1 (the 5V fixed version). I plan…
Part Number: LMR43610 Tool/software: Hello, I have implemented a voltage regulator that converts a voltage ranging from 4V to 36V to a fixed voltage of 5V based on LMR43610R3RPER. The maximum current delivered by the regulator is 1.2A. Below is the schematic…
Part Number: LMR43610 Other Parts Discussed in Thread: LMR36501 , Hi team,
Is it possible for LMR43610 and LMR36501 to change the output voltage by the external DAC like the figures below?
Best regards,
Shunsuke Yamamoto
Part Number: LMR43610 Tool/software: Hi,
Question 1: The input voltage of LMR43610 is 15V, the output voltage is 1.8V, and the load current is about 100mA. What is the approximate efficiency? Question 2: The input voltage of LMR43610 is 15V, the output…
Part Number: LMR43610-Q1 Other Parts Discussed in Thread: LMR43610 Tool/software: Hi Team,
We tested the short-circuit protection function of the LMR43610 and would like to confirm whether it is working correctly.
The waveform is shown below.
The…