Part Number: LMR43610 Hi,
I am planning to design a Step-Down circuit using the LMR43610MB3RPER.
Vin: 4.8~36V
Vout: 3.3V
Iout: 0.3A
Ripple Current Ratio K = 0.3
Using the inductor calculation formula provided in the datasheet, I found that when Vin…
Part Number: LMR43610-Q1 Hello Team,
one question rised up:
Is the PGOOD logic block of the LMR43610-Q1 Independent from EN-pin?
Means if EN pin is de-actived also PGOOD will be switched off (driven by the EN-logic)
or
is PGOOD a comparator logic which…
Part Number: LM5152-Q1 Other Parts Discussed in Thread: LM51521-Q1 hi Friend,
I want to know the difference between LM5152-Q1 and LM51521-Q1. in the datasheet ,what means of Bypass Operation?
Hi Shihui,
You are welcome! SCH is in below evm user guide. The buck converter IC was changed to LMR43610MSC3RPERQ1 during test.
LMR43620-Q1 EVM User's Guide (Rev. B) (ti.com)
BR,
Victoria
Part Number: LMR43610 Hi,
Is it possible to use a LMR43610MB3RPER in adjustable mode to make a 9,5V rail (from a 13V input), the datasheet is a bit ambiguous with respect to this. It says that Adjustable is possible, but only shows 4 parts in the part…
Part Number: LMR43610 Hello, TI team! A step-down stabilizer is needed: Input voltage 3.3 V - 7 V. Output voltage 3.3 V. What is the input current of the LMR43610 at a load current of 5 - 10 µA? Thank you!
Part Number: LMR43610-Q1 Hi Team,
LMR43610MSC3RPERQ1, Standby IQ(mA)
Q1: Test condition is VEN = 0V ?
Q2: Is 3.3V/Adjustable also applicable to this specification?
Thank you.
Part Number: LMR43610-Q1
Hi!
Can you help me to review the Volvo Group BMS prototype board schematic?
They will use the LMR43610RS5QRPERQ1
Output current ~100-200 mA max
Besides the missing Vin 100nF input capacitor it looks ok?