Part Number: LMR43610-Q1 Hi Team,
Please help proide efficiency figure for part number :LMR43610MSC3RPERQ1,OUTPUT CURRENT :1A,OUTPUT VOLTAGE :3.3V Fixed /Adjustable,EXTERNAL SYNC :Yes (PFM/FPWM Selectable),FSW :Fixed 2.2 MHz,SPREAD SPECTRUM :Yes
Thank…
Part Number: LMR43610-Q1 Hi, please could you check my schematic and layout? This is for a 5V output with 1A max (More likely to be 500mA)
/resized-image/__size/960x720/__key/communityserver-discussions-components-files/196/5V_5F00_3D.png - 3D
/resized…
Part Number: LMR43610-Q1 The chip achieves an output voltage of 9V, when the input voltage is lower than 9V, what does the output voltage look like? Will it follow the decrease? What is the minimum no-drop time to be satisfied?
Part Number: LMR43610-Q1 Other Parts Discussed in Thread: LMR43610 , Hi Team,
We considering use LMR43610RS5Q , could you kindly help with following questions?
Vin:12V
Vout:5V
Current: 20mA ~ 250mA variation
My Question:
Q1:How much current LMR43610RS5Q will…
Part Number: LMR43610-Q1 Dear TI team,
I have a weird behaviour of LMR43610MSC5RPERQ1 if configured in adjustable mode (with 39.2k / 10k divider as in the partial schematic below).
DC/DC, when loaded, is working well if VIN>10V, but output voltage is…
Part Number: LMR43610 Other Parts Discussed in Thread: LMR43620 Hello,
Does TI have effiiciency data for the LMR43610 at 3.3Vout?
Also, are there any plans to release a 3.3Vout version of LMR43620?
Thanks,
Michael
Part Number: LMR43610-Q1 Hi, I saw on the datasheet that the absolute maximum rating is 42V, however there is a larger ESD value. I am thinking of having this supply voltage from a 23-32V DC PSU to my PCB, will these values of suppression and circuitry…
Part Number: LMR43610-Q1 Hello Expert,
I'd like to confirm about output accuracy during Auto-mode
At FPWM mode, datasheet said that accuracy will be 4.94~5.00~5.06V.
Also, datasheet said set voltage during auto mode will be 1% higher.
Then, Could…