Part Number: LMR43610-Q1 Hi Team,
Please help proide efficiency figure for part number :LMR43610MSC3RPERQ1,OUTPUT CURRENT :1A,OUTPUT VOLTAGE :3.3V Fixed /Adjustable,EXTERNAL SYNC :Yes (PFM/FPWM Selectable),FSW :Fixed 2.2 MHz,SPREAD SPECTRUM :Yes
Thank…
Part Number: LMR43610-Q1 Hi, please could you check my schematic and layout? This is for a 5V output with 1A max (More likely to be 500mA)
/resized-image/__size/960x720/__key/communityserver-discussions-components-files/196/5V_5F00_3D.png - 3D
/resized…
Part Number: LMR43610-Q1 Other Parts Discussed in Thread: LMR43610 , Hi Team,
We considering use LMR43610RS5Q , could you kindly help with following questions?
Vin:12V
Vout:5V
Current: 20mA ~ 250mA variation
My Question:
Q1:How much current LMR43610RS5Q will…
Part Number: LMR43610-Q1 Dear TI team,
I have a weird behaviour of LMR43610MSC5RPERQ1 if configured in adjustable mode (with 39.2k / 10k divider as in the partial schematic below).
DC/DC, when loaded, is working well if VIN>10V, but output voltage is…
Part Number: LMR43610-Q1 Hi, I saw on the datasheet that the absolute maximum rating is 42V, however there is a larger ESD value. I am thinking of having this supply voltage from a 23-32V DC PSU to my PCB, will these values of suppression and circuitry…
Part Number: LMR43610-Q1 Hello Expert,
I'd like to confirm about output accuracy during Auto-mode
At FPWM mode, datasheet said that accuracy will be 4.94~5.00~5.06V.
Also, datasheet said set voltage during auto mode will be 1% higher.
Then, Could…
Part Number: LMR43610-Q1 Hi, Please could you check that my scheamtic and PCB layout for this component for a 5v fixed outout.
Schematic -
PCB 2D view -
PCB 3D -
Thank you!
Part Number: LMR43610-Q1 Other Parts Discussed in Thread: LMR43620 , LMR43610 we need to observe the functionality of the IC (Adjustable Output voltage configuration ,ripple). It will be helpful if we can have the Pspice or Tina TI simulation model.
Part Number: LMR43610-Q1 Other Parts Discussed in Thread: LM61480-Q1 Hello TI,
We are checking the input range of LMR43610-Q1, and wondering if there is a specification of VIN sustained to transient like LM61480-Q1 list in datasheet? Thank you.
LM61480…