Part Number: LMR43610-Q1 Hi team,
My customer needs to know our light load efficiency data. Could you please help to test according to the excel data?
The part number is LMR43610RS3QRPERQ1, PFM, Fsw=400k.
Thanks for your support!
Copy of LMR43610 light…
Part Number: LMR43610-Q1 Other Parts Discussed in Thread: TPS560430 Hi team,
Could you advise a definition of "thiccup" value in the datasheet?
Please advise the condition at which hiccup is triggered.
regards,
Part Number: LMR43610-Q1 Hi team,
Could you advise the difference between VDROP1 and VDROP2?
I think VDROP2 is the VIN to VOUT difference with Fsw>1.85MHz and 95% regulation.
But there is no frequency condition in VDROP1. Does it mean VDROP1 assumes…
Part Number: LMR43610-Q1 Hi team,
Could you advise the Fault recovery condition from Vout UV fault?
It is described in the datasheet as below
V PGDUV + V PGDHYST < V OUT <V PGDOV -V OGDHYST
V PGDUV = 89% to 94.2%
V PGDHYST = 1.1% to 5.9%
Is the worst case…
Part Number: LMR43610-Q1 Good day
We are using a non-Q variant of the LMR436x0 in a design and I am trying to make sence of the datasheet i have for that. In the latest datasheet of the Q variant, snvsbe0e.pdf, there is a requirement for the parallel…
Part Number: LMR43610-Q1 Other Parts Discussed in Thread: LMR43610 Hi,
1.
I'd like to know quiescent current for LMR43610 , with output voltage as 5V.
Above is the Non-switching input current specified in Electrical Characteristics in LMR436x0-Q1 datasheet…
Part Number: LMR43610-Q1 Dear Team
There is a new demand from our custom:
1.Input: 9-36V
2.Output: 6V/0.6A
3. Quiescent Current Iq must be lower than 70uA with 50uA load with output load.
From datasheet we could know that Iq of LMR43610-Q1 is 1.5uA , but…
Part Number: LMR43610-Q1 Other Parts Discussed in Thread: LM53601-Q1 , Hello,
In our DS we have a formula for Iqvin but do not have a value for Ibias that I can find. Am I just missing it or is it the Ifb(lkg) number? In other datasheets like LM53601-Q1…
Part Number: LMR43610-Q1 Other Parts Discussed in Thread: LMR43610 , TLVM13620 We need a power conversion chip, the input voltage range is 6VDC ~ 18VDC, the output 5V/1A, need to have enable port, can control the chip through the external enable signal…
Part Number: LMR43610-Q1 Hi team,
Is there any concern if I use 0.22uF(220nF) for Cboot instead of 100nF which is recommended in the datasheet?
regards,