Part Number: LM61495 Other Parts Discussed in Thread: TPS62067 , TPS568215 , TPS65023 , , TPSM63610 , LMR43620 , TPSM33625 Tool/software: Hi Team,
As per below suggestion (image), it is recommended to use the following combination of three ICs for…
Hi Nikhil,
I can recommend the LMR43620 for a 24 to 5 V 1.5 A application. It is available in both auto and industrial trims and provides a good mix of ease of use, solution size, efficiency, and EMI performance among other features.
Thank you,
…
Hi,
As the load is very small, it's suggested to test on the EVM to get the efficiency data. Also if you want to get higher efficiency, you can take a look at LMR43620-Q1 for the 1.8V rail. For TPS65320, you need to contact the IPP-PMIC team for more…
Part Number: LMR34215-Q1 Other Parts Discussed in Thread: LMR33620 , LMR43620 , LMR33610 , LMR36015 Hi,
My Requirement is 6V-36V Input, 5V Output, 1A Output, Ambient Temperature is (-40degC to 90degC). Can you please suggest any part which meets all…
Hi Will,
To meet your requirement, the best option related to the LM61430-Q1 would be to use a two chip solution of an LMR43620-Q1 for the 3.3V/2A and an LMR43610-Q1 for the 5V/500mA.
Best regards,
Ridge
Hi Shihui,
You are welcome! SCH is in below evm user guide. The buck converter IC was changed to LMR43610MSC3RPERQ1 during test.
LMR43620-Q1 EVM User's Guide (Rev. B) (ti.com)
BR,
Victoria
Hi Oba,
Oba said: My customer is asking me if this kind of table is availbale for LMR14020. Do you have anything? Or is component calculator availble?
Unfortunately, we do not have a calculator or anything showing BOM options for the LMR14020.
Oba…
Hi, Hareesh,
The design look good to me without big issue, suggest to increase Cout, and input 0.1uf is better to have.
below is Webench result, you can also take as reference.
BTW, if this is your new project we strongly recommend new device LMR51420…
Part Number: LMR43610-Q1 Other Parts Discussed in Thread: LMR43620-Q1 Hi team,
Could you give me a guide line and restrictions for selecting the LC filter of LMR43610-Q1 at 2MHz?
I plan to use LMR43610-Q1 at 2MHz 1.0A maximum and 0.22A typical.
…
Part Number: BQ25731 Other Parts Discussed in Thread: BQ25730 Dear Madam/Sir,
I would like to have your eye on the design review (on PDF page 11) (P9DF page 8 is power tree)
One more question, could I direct output Vsys to PMSM Motor (24V)? rectangle…