Part Number: LMR50410 Tool/software: Hello
We are experiencing the destruction of processors being supplied 3v3 from a LMR50410XFDBVR device. It happens very occasionally. The circuit around the LMR50410XFDBVR is pretty much the recommended schematic…
Part Number: LMR50410-Q1 Tool/software: Hi team,
Could you tell me the JEDEC High-K board design for this device to spec out the D/S thermal impedance?
This information is quite helpful to quantitatively understand why the actual performance(such…
Part Number: LMR50410 Tool/software: Hi,
We have a customer who ordered 6000 pieces of LMR50410Y5FQDBVRQ1 on 26 Jan 2024.
Date code: 2310M
Lot code: 3200872PHI
They would like to confirm if the changes in the attached PCNs are applicable to these…
Part Number: LMR50410 Tool/software: Hi,
I'm designing a power circuit with a 24V input and three different DC outputs: 12V, 5V, and 3.3V. I'm considering using non-isolated buck converters for simplicity, as they don't require a flyback transformer…
Part Number: LMR50410-Q1 Hello
Is there a reference schematic for the fixed output version of LMR50410-Q1? The schematic on page 17 of the datasheet appears to be for the adjustable version.
I'm looking to use the 5 volt fixed output version.
Thanks…
Part Number: LMR50410-Q1 Tool/software: Dears,
in some platforms/finished PCBAs equipped with your device with part number LMR50410YFQDBVRQ1 we are planning the application of Conformal Coating for the typical known scopes (protection from moisture…
Part Number: LMR50410-Q1 Tool/software: we have connected the circuit as per datasheet, our input voltage is 5V which we have given through USB and that is reflecting in the input side, but for the output side we need a voltage of 3.3V, the feedback resistors…
Part Number: LMR50410-Q1 Other Parts Discussed in Thread: LMR50410 Hi,
I recently submitted a product for EMC testing using the LMR50410. The design of the regulator was copied almost identically from the EVM module. The product failed radiated emissions…