Part Number: LMR50410-Q1 Tool/software: Team-
A customer would like to use LMR50410-Q1 with Vin=24V, Vout = 15V and 5V.
Page 17 of the datasheet has a nice table of recommended component values but for Vin=12V.
Can you please make suggestions (would…
Part Number: LMR50410 I'm a little bit confused about choosing a suitable inductor for my fixed output 3.3V version of the buck converter.
the data sheet recommends a 10uH Inductor _I chose that one "MPL-SE2512-100"; ad here is a link for its specs…
Part Number: LMR50410-Q1 Hi team,
Datasheet shows the efficiency versus load current like below, for both PFM and FPWM. For the load larger than 0.1A, it looks only the data for FPWM is shown. But I believe the efficiency for PFM and FPWM is the same…
Part Number: LMR50410-Q1 Hi all,
In datasheet section 9.2.2.5, it mentioned a part of output ripple is "caused by the inductor current ripple charging and discharging the output capacitors", and the following equation is given. I had some trouble…
Part Number: LMR50410 Hi,
As for the feedback reference voltage Vref, the data sheet states that Rfbt and Rfbb should be set so that the accuracy is ±1%. If the resistance value varies due to changes in resistance value accuracy and temperature characteristics…
Part Number: LMR50410-Q1 Other Parts Discussed in Thread: LMR50410 Hi Team,
There is a good new that we DIN LMR50410-Q1
And there have one thing need your support!
1. If Vin is 8V , what Vout_max of LMR50410 can be? It's 7.84V?
2. What are the…
Part Number: LMR50410 Other Parts Discussed in Thread: LMR54410 , , LMR14010A , LMR51610 Hi support team,
The LMR54410 has the function of "Replacing Non Sync Converter".
Does LMR50410 have this function? Can I replace the LMR14010A?
Regards, Dice…
Part Number: LMR50410-Q1 Hi Team,
My customer is using the LMR50410-Q1 in the On board charger. And they ask us if the RC filter at SW pin is ok to be added. I haven't clarify the reason why customer want to add this modification, but very likely it…