Part Number: LMR51403 Hi,
I have inherited a simple 12V Lead acid battery charger design using the LMR51403XDBVR powered from a 24V DC supply.
The design makes use of the internal current limit to restrict the charging current to ~ 400ma, the voltage…
Part Number: LMR51403 Hello Team,
I have designed buck converter for our railway application having below specification
Vin min 11V Vin Max 13.2V
Vout 10V
IOut 300mA
As I will need maximum duty cycle of 95% device will enter frequency foldback…
Part Number: LMR51403 Hi all,
I am using the LMR51403X EN input as an undervoltage lockout in an ultra-low-power application.
I have the problem that the voltage at which the buck-converter turns off is not what I expect it to be.
The root cause…
Part Number: LMR51403 Tool/software: Hello TI community,
I consider using LMR51403 in a battery monitor application due to its nice PFM/FPWM feature. Can you please support by providing simulation models (even if not finally validated; webench or pspice…
Part Number: LMR51403
Tool/software:
Dear Team,
I am using LMR51403 for buck converter where Vin is 11V and Vout is 10V due to required high duty cycle buck will go to frequency foldback mode of operation.
Is this ok if we continuously use buck…
Part Number: LMR51403 Tool/software: Hello I need to have the output voltage of thr buck converter to be adjustable on the fly by a microcontroller application.
A common approach is to inject an additional current through a DAC and a resistor to the…
Part Number: LMR51403 Tool/software: Dear Team,
Why this LMR51403 buck converter shall not be used in continuous foldback frequency mode in a case where large duty cycle needed ? Due to what parameters it could get fail ?
Thank you.
Br,
Vai…
Part Number: LMR51403 Tool/software: Dear Team,
I am using LMR51403 for below requirement :
Vin 12V
Vout 10V
Vout 300mA
From my calculations:
L 120uH
lseries inductance is 170mOhm
As device will go into frequency foldback mode due to…
Part Number: LMR51403 Tool/software: Hi team,
As we knew LMR51403YFDBVR is a 1.1MHz device,
is the frequency always fixed at 1.1MHz? Or customer can change the inductor and Co to make fsw=800kHz?
They think 1.1Mhz is too fast. Thanks
Part Number: LMR51603EVM Other Parts Discussed in Thread: LMR51403 , , LMR51603 Tool/software: Hello guys,
One of my customers is considering using LMR51403 for their new products.
But LMR51403EVM has been not released. At this moment, they have the…