Part Number: LMR51420 Tool/software: Hi team,
Customer found output surge is big to generate EMI and wants to implement RC snubber circuit. Do you have recommendation for Snubber and layout?
Regards,
Hayashi
Part Number: LMR51420 Tool/software: I am using LMR51420 to generate 5V from 24V. This 24V is generated from a smps supply with primary side regulation topology Having output cap of 4500uF. 24V is transferred to LMR51420 VDD pin via 2-pin Connector. Normally…
Part Number: LMR51420 Other Parts Discussed in Thread: LM61460 Tool/software: Hello,
My customer has doubts about the thermal characteristics of LMR51420.
Compared to other products that generally have GND on the bottom side for thermal temperature…
Part Number: LMR51420 Tool/software: PSpice simulations are running very slow on the new laptop.
Simulation times for same project:
Old laptop Win11: Intel XEON W-10885 CPU @ 2.40GHz Simulation time 30 minutes.
New laptop Win11: 13th Gen Intel Core…
Part Number: LMR51420 Other Parts Discussed in Thread: LM2841 Hi team,
Whether 51420 EN pin can realize the shutdown function of LM2841?
Thanks
Lillian
Part Number: LMR51420 Tool/software: I design circuits using TI Power Design(Power Designer (ti.com)).
Detal: Vin:24V Vout:12V Iout:2A
I chose the following design.
The chip (LMR51420) shorted out when it was powered on。Why?
After adjusting…
Part Number: LMR51420 Tool/software:
Hello,
In my schematic, I use the LMR51420 component to precharge my large 1000µF capacitors. My 24V input is switched abruptly by a mechanical switch. When my output voltage becomes close to the input voltage…
Part Number: LMR51420 Tool/software: Dear Specialists,
My customer is evaluating LMR51420EVM and has questions.
I would be grateful if you could advise.
---
When the LMR51420YFDDCR is turned on with a light load (about 100mA), the inductor current…