Part Number: LMR51430 I am currently designing a customer's circuit. If VIN is lower than the voltage set on FB, is it okay to think that VOUT will be output at around VIN x 0.95? Also, will any problems occur if I continue to use it in this condition…
Part Number: LMR51430 Other Parts Discussed in Thread: LMR14030 , , LMR33640
Hello There, I'm looking to port a LMR14030 design to LMR51430X for12-36v Input to 9v Output conversion. I'm facing some issues with the initial testing. With no load, multimeter…
Part Number: LMR51430 Other Parts Discussed in Thread: TPS563252 , Hi team,
Schneider encountered a problem in IC selection and would like to inquire whether LMR51430 can be used instead of TPS563252.
The application is to power radio frequency devices…
Part Number: LMR51430 Customer is trying to evaluate the device with specific conditions. After evaluating it by WeBENCH, it shows exceed the temp and doesn't work.
May i know the criterion detail. what's the limitation? is it TJ?
Regards
…
Part Number: LMR51430LMR51430 support,
I went through the equations in section 9.2.2.4 of the datasheet, and the value for the inductor selection is different from the result given in the datasheet. It looks like the calculation is based on a Vin Max…
Part Number: LMR51430 Other Parts Discussed in Thread: TLV62569 Team, I'm confused about the voltage derating 38V,max for SW_Transient <20nS. Why is it 38V at this condition? Is that correct?
Regards
Brian
Part Number: LMR51430 Hi,
can the LMR51430 handle the situation when there is no input voltage but the output voltage (at the output capacitors) stays at a certain level, say 5 volts, which are supplied from another source? Or should I decouple the output…