Part Number: LMR51450 Hi,
Kindly review the attached schematic, let us know if any major comments are there to change.
Reuirements :
VIN=4.8V
VOUT= 4.2V
Current = 2 A
Regards, Saurabh Keshari
Part Number: LMR51450-Q1 Other Parts Discussed in Thread: LMR51450 Hi ,
Please review the below circuit and let me know any improvization needed to obtain more reliable design.
I am unable to upload the file. keep througing the error.
The schematic…
Part Number: LMR51450 Tool/software: Hi,
In our board use LMR51450 for 2 application, one is 12V DC2DC output ,another is 5V DC2DC output, both 24V DC input.
12V DC2DC with loading, but 5V DC2DC is reserved function without any loading . We found…
Part Number: LMR51450 Tool/software: Hi,
Is LMR51450SQDRRRQ1 a drop-in replacement for LMR51450SDRRR? Do you have a specification compare to show the subtle difference between the two parts? Thanks.
Best regards
Gordon
Part Number: LMR51450-Q1 Hi,
I have considered the LMr51450-Q automotive grade DC-DC switching converter (Integrated FET) for one of our new product developed design. The requirements are given below,
Input : 12VDC (Regulated) (or) 9V battery input…
Part Number: LMR51450 Tool/software: HI, All,
We encountered a horrible problem with the LMR51450 enable pin。
Our products use the LMR51450 switching regulator as a 24V to 12V power conversion controller。
However, I made the mistake of leaving the…
Part Number: LMR51450 Tool/software: Hi,
I am trying to evaluate the implementation of LMR51450. The only model provided is a Pspice encrypted model so I am using PSpice to run the simulation.
Every time i run the simulation it takes around 4 hours…
Part Number: LMR51450 Tool/software: Hi, I am using the LMR51450 as a 12V buck converter for a 4S li-ion battery (12.8V-16.8V). I followed the schematic and recommended component values as mentioned in the datasheet, but the output of the buck converter…
Part Number: LMR51450 Hi
Is it possible to make an inverting buck converter using LMR51450?
The device is internally compensated, can this work for inverting buck as well?
The device is syncronous rectified, is that compatible with inverting buck…
Part Number: LMR51450 Hi team,
My customer is considering to use LMR51450SDRRR.
In the recommended operating conditions, it is mentioned that maximum DC load current is 5A, but it may be derated when operating with high switching frequency and/or…