Part Number: LMR51610-Q1 Tool/software: Hello,
For a 5V output with the LMR51610-Q1, the datasheet selects a 22.1k resistor for RFBB and calculates 118k for RFBT accordingly. In Webench, however, it suggests 19.1k for RFBB and 100k for RFBT. Both combinations…
Part Number: LMR51610-Q1 Other Parts Discussed in Thread: LMR51606 Tool/software: Hello,
We are using LMR51610-Q1 for our project that;
Vin shall be around: 8-32V
Vout and Iout shall be 5V and 200mA
Our PCB shall be very small so we have to make…
Part Number: LMR51610-Q1 Other Parts Discussed in Thread: LMR51610 Tool/software: Hello,
In our projects, we are using the LMR51610 SMPS.
The IC enables when Vin is around 4.5V to 5V. I have connected the EN (Enable) pin to VIN through a 100k resistor…
Part Number: LMR51610-Q1 Tool/software: Hello, in our project we are using LMR51610-Q1 with the parameters:
Vin : 8-32V
Vout: 5V
Iout: 1A
Could you validate the schematic?
Additionally, 22u 10V out capacitors ordering code is CL31B226KPHNNNE…
Part Number: LMR51610-Q1 Other Parts Discussed in Thread: LMR50410-Q1 , LMR50410 , LM5166 Tool/software: Trying to create a design using the Type 3 Ripple Generation Method using the LMR5166-DESIGN_CALC_REVA1 calculator.
(1) The LMR516XX-DESIGN_CALC_REVA1…
Part Number: LMR51603-Q1 Other Parts Discussed in Thread: LMR51610-Q1 We referred two part numbers LMR51603-Q1 LMR51610-Q1 We are converting 16-32V to 12V output When referring the datasheet for 12 V output we found two different values for the inductors…
Part Number: TPS63710 Other Parts Discussed in Thread: LMR51610-Q1 Tool/software: I need a converter which converts +24V to -15V.Kindly provide me with a list of parts that matches the above specification.
Hi Onkar. Thank you for reply.
for your information, the part we want to use in our product is the LMR51610-Q1.
In our prototype, using LMR51610XFDBVR and LMR51610YFDBVR.
Regards
Part Number: LMR51603-Q1 Other Parts Discussed in Thread: LMR51603 , LMR51610 Tool/software: Hello,
Is there any simulation tools available with that dc/dc converter ?
Best regards