Part Number: LMR54410 Hi,
One of our customers has the following question:
"Can you provide us with the unencrypted Spice model of the LMR54410, both with and without the -F suffix?"
Do we have the models and could you please attach them here…
Part Number: LMR54410 Other Parts Discussed in Thread: LMR51610 Do you have an otherwise equivalent one with an input voltage of 60V instead of 36V with an output voltage of 12V/24V 1A?
Part Number: LMR54410 Other Parts Discussed in Thread: , TPS54J061 , TPS62933 , LMR14020 , TPSM5601R5H I have the following questions on this IC and the LMR54410 EVM:
Is stability guaranteed if used as "normal buck" with recommended L & COUT? The…
Part Number: LMR54410 Tool/software: Dears,
I am recenty trying to placea sample order for the following items: LMR54410DBV TLV75733PDBV TLV75730PDBV PCM5102APWR Unfortunately, no chance to finish checkout, and there is a note "You can order samples…
Part Number: LMR54410 Hello, the diagram for our circuit using the integrated circuit LMR54410DBVR is shown in the image below.
When the circuit has to be powered by 5 volts (USB, via connector J1) , there is still a diode D10 adding a drop of approximately…
Part Number: LMR54410 Other Parts Discussed in Thread: TPS560430 Tool/software: Dear Support, We want to simulate FRA (AC Bode plot) operation of LMR54410(F), but operating in constant current mode, with current-sense amplifier in feedback loop. Something…
Part Number: LMR54410 Tool/software: I am currently supporting one of our prospects on an EMI/EMC-related pilot project , in which they are using the LMR54410DBVR buck converter IC from Texas Instruments. As part of the simulation workflow, we are required…
Part Number: LMR54410 Tool/software: Hi Team,
I wished to design a module which supports 3.3V, 5V 12V and 24V output voltage with minimal design variants. As per the datasheet and webench, inductor values suitable are,
Output Voltage
Inductor…
Part Number: LMR54410 Dear team,
We are referring the datasheet of LMR54410 and it mentions below.
In genral lower layer PCN should have higher thermal resistance but it mentions opposite. It is not simple 4-layer vs. 2-layer but JEDEC 4-layer vs…
Part Number: LMR54410 Tool/software: We have ordered the part LMR54410FDBVR and on TI website (also in Datasheet) this part is declared as MSL 1 but the part we have received has MSL 2 written on the label.
Now I'm not sure if I should trust the Data…