Part Number: LMR60410-Q1 Other Parts Discussed in Thread: LMR60410
Hi
Please help to review the design circuit about LMR60410-Q1, automotove use:
And another question is, LMR60410-Q1 no adjustable version? Just fix voltage value version for select…
Part Number: LMR60410-Q1 Other Parts Discussed in Thread: LMR60410 TI - There is an appnote "How to Modify a Step-down Converter to the Inverting Buck-boost Topology"
I am wanting to use the LMR60410 step-down converter and convert from a lithium ion…
Part Number: LMR60410 Hi E2E support
My customer is interested in the LMR60410. Could you please let us know if you have any information on when the other options (Preview devices) will be available for ordering?
LMR604105SRAKR (preview) LMR604103RAKR…
Part Number: LMR60410 Hi team,
Is this device possible to use as inveting buck boost converter? Based on the sentence below, it is impossible to do so.
Best regards,
Shunsuke Yamamoto
Part Number: LMR60410 I am using LMR60410 as a power source for a camera deserilizer PoC Power Over Coax network with 12V input and 11V output. " The PoC network can support up to 300mA of current" is mentioned in the datasheet. So how can I limit the…
Part Number: LMR60410-Q1 Other Parts Discussed in Thread: LMR60410 Hello TI Support Team,
Please find attached our schematic design based on the LMR604105SRAKRQ1 for a 24V input and 3.3V fixed output application.
Could you kindly review the schematic…
Part Number: LMR60410 Tool/software: When using the LMR604103SRAKR DCDC, with an input of 5V and an output of 4.5V, when carrying a load of 1A, the output voltage is only 4V, and the voltage drop is relatively large. What is the reason for this? How should…
Part Number: LMR60410-Q1 Hi team,
The dimensions of the PAD described in DS are too difficult to understand. Please help confirm the dimensions of the PAD in the image below.
Part Number: LMR60410-Q1 Forword: This is more of an observation than a complaint as I believe I have figured out my problem.
I have fried two of the same rail regulators on my rev1 boards (which uses a total of three LMR604103SRAKRQ1's, one for 10v…
Part Number: LMR60410 Tool/software: Hello,
while redesigning our unit I have came across LMR60410. It seems very promising, however I would like to verify one aspect I have not found documented well and the LMR60410QEVM development kit is hard to obtain…