Part Number: TPS61381-Q1 Other Parts Discussed in Thread: LMR71915 , LM5013 I have an application that requires a 13Vdc @1Adc power rail. This will be provided from a LMR71915 or LM5013 buck converter. I would like to back this up using the TPS61381 or…
Part Number: LMR71915 Tool/software: Hi Team,
As title, I plan to use LMR71915 at input voltage range from 18V-75V and output 3.3V/1A.
Question is the power input circuit placed a TVS diode with maximum clamping voltage as 121V to protect the downstream…
Part Number: LMR71915 Other Parts Discussed in Thread: TPS61175-Q1 hi sir
we need a solution ,
spec as below:Vin:9~60v, vout:38v/200mA
first stage use the LMR71915 down to 5V
second stage use the TPS61175-Q1 , from 5v boost to 38v/200ma
Does…
Part Number: LM65635 Other Parts Discussed in Thread: LMR71915 , LM5169 , LM5168 , LM5160 , LM5166 , LM5032 I am looking for Buck DC-DC Isolated solution.
I/P: 16V- 50V, 15W
O/P Main 5V , 7.5 W
O/P Aux +- 15V , 7.5 W
Please suggest the solution…