Pradeep,
The EP version stands for "Enhanced Product" ( more info on EP ). It is hi-rel and has enhanced specs such as operating temp down to -55C vs -40C.
SWIFT is a trademark name for some of our DC/DC converters.
EP should not have better or…
Are you open to use this part (LMS3655) for your 5A design? Abs max for this part is 40V
www.ti.com/.../LMS3655
This part is designed for low EMI type of design with spread spectrum also available.
Otherwise, with non-synchronous design the switching…
Part Number: LMR23630-Q1 Other Parts Discussed in Thread: LMR23625 , LMS3655 Hello TI,
What precautions should be taken when placing two LMR23630s side by side? Do I place them orthogonal to each other or parallel? The Vin and Vout paths are similar to…
Part Number: LMS3635-Q1 Other Parts Discussed in Thread: LMS3655-Q1 , Hi
Please let me ask you about LMS3635-Q1 or LMS3655-Q1.
1. Are there the conducted EMI data without the spectrum spread function
2. Are there the conditions to change form PWM to PFM…
Hello,
A similar response applies for LM43603 input capacitors as the LMS3655. It is recommended to use a high frequency capacitor and a lower value bulk ceramic (ie. 4.7uF) with both ceramics placed close to device along with a larger bulk capacitor…
Part Number: LM73605-Q1 Other Parts Discussed in Thread: LM73605 , LMS3655 Hi Team,
I am currently working on a reference design where I would like to design in an LM73605-Q1 to support an application where the input can range from 9V-30V and the output…
Part Number: LMS3655 Hi, I need a negative converter design used to function as a preregulator for an negative regulator/LDO in a power supply design. I am using a LLC converter/transformer with center-tapped secondary to step the voltage down to +/- 24V…