Part Number: LMT87-Q1 Other Parts Discussed in Thread: LMT87 , LM94022
End of Life
PTN (Part Termination Notice) period
Life & BCP (Business Continuity Plan)
Generation & Technology
Alternate parts - EOL
-PTN
-Life…
Part Number: LMT87 Other Parts Discussed in Thread: LM34 , LM35 , , THVD1400 Tool/software: Hello E2E Community,
We are reaching out to re-confirm if LMT-87 can be used in 2-wire configuration the way LM35/34 have been configured in application note…
Part Number: LMT87 Other Parts Discussed in Thread: ISOTMP35 Tool/software: Hi team,
Below is an question from customer. Could you help to take a look?
What is the maximum voltage applied on the plastic cover of LMT87, or what is the isolation voltage…
Part Number: LMT87-Q1 Dear,
we found there are 2 different shape in the same tape for LMT87QDCKRQ1, and checked many different DC, no matter 21+, 22+ or 23+ all has this issue, so could you indicate if it's general situation?
Part Number: LMT87 Hi team, I'd like to know about the pin one designator for SOT devices. PCN(20240203000) said current is Pin One Stripe only. The 2 year old device we have is a Pin one Dot. Is this a PCN mistake? BR, Kengo.
Part Number: LMT87
Tool/software:
Hello E2E Team,
We are planning to use LMT87 for our remote temperature measurement use case with sensor being encapsulated inside a SS Metal Probe.
I want to understand for a CAT6 Twisted pair cable length of…
Part Number: LMT87 Hello everyone,
What was the VDD value used to create the data in Table 3 ("LMT87 Transfer Table") in LMT87.pdf?
I do not see the value of VDD used to create the data in Table 3 ("LMT87 Transfer Table") in https://www.ti.com/lit…
Part Number: LMT87
Tool/software:
Hello E2E Community,
We are considering the TO-92 Package of the LMT87 sensors for our remote temperature sensing use case for bearing temperature monitoring.
I however would like to know if this package is suitable…
Part Number: LMT87
Tool/software:
Hello E2E Community,
We are planning to use LMT87 in TO-92 package for remote temperature sensing use case. We want to minimize the number of components installed near the sensor & hence this query.
We plan to…
Part Number: LMT87-Q1 Good day colleagues,
Can you tell me whether the temperature measurement of the LMT87-Q1 is carried out via a specific pin, or whether all pins are equally well thermally connected to the sensor?
Thanks,
Daria