Hello Given,
The link below shows all analog sensors which support -40C to 150C and are available in SC70(DCK) 5 pin package. TMP9A00-EP is the only device with the same gain of -11.77mV/C. If you can use a different sensor gain, TMP235 is a good candidate…
Other Parts Discussed in Thread: LMT87-Q1 , TMP112-Q1 Hi Team,
Customer is currently using this LMT87-Q1 temperature sensor for one of our applications. He was curious about the worst-case temperature accuracy for this component. Table 7.5 in the datasheet…
Part Number: LMT87-Q1 Hi Champs,
Regarding to LMT8x-Q1 device, my customer asks following questions.
LMT8x-Q1 measurement range and Tj-max are the same. Is it OK that LMT8x-Q1 put in 150C ambient temperature?
What kind of failure would occur if LMT8x…
Part Number: LMT87-Q1
Hi there,
I'm calculating the thermal characteristics of LMT87QDCKTQ1 and found the equation below in the datasheet (page 11):
Tj = Ta + Tja.[(Vdd.Is) + (Vdd - Vout ).IL]
In the same page below the equation, there's an example…
Hello Kelvin-san,
Thank you for your answer.
I’m suggesting LMT87-Q1 and TLV3201-Q1 to perform temperature switch with large hysteresis (100C ON and 30C OFF) to customer.
So I wanted to confirm that LMT87-Q1 output doesn’t behave like green…
Other Parts Discussed in Thread: LMT87-Q1 , MANDO Hi,
I'm FAE in TI Korea Automotive and support Mando account. EPS team in Mando is evaluating LMT87-Q1 and recently requested PSPICE model. Could you provide this?
Best Regards,
Ian
Other Parts Discussed in Thread: LMT87-Q1 Hello together,
are there any test-results available which evaluates the long-term-stabiltiy of the LMT87-Q1?
In addition, will the accuracy degrade after the soldering-process?
Thanks in advance for your help…
Other Parts Discussed in Thread: LMT87-Q1 , LMT84-Q1 , LMT87 Hello,
LMT87-Q1 datasheet page 4 has ACCURACY CHARACTERISTICS and only following temperature range has maximum value of 2.7°C.
70°C to 150°C; VDD = 3.0 V to 5.5 V
0°C ; VDD = 3.0…
Other Parts Discussed in Thread: LMT87 Hello,
Datasheet explain “11.2 Layout Example” and 3 VDD are connected to power plain.
But I need to connect only 1 VDD to power plane like attached file because of layout restriction.
E2E_LMT87-Q1.p…
Part Number: LMT86 Other Parts Discussed in Thread: TMP235
Team,
Apart from the different LMT86 OPNs ( LMT86 vs LMT86-Q1 ) do we have some P2P dropped-in alternatives for LMT86QDCKRQ1 ? Apart from the mV/Deg C difference what would need to be taken into…