Part Number: LM4040-N-Q1 Other Parts Discussed in Thread: LM4040-N Tool/software: I'm currently using a zener diode to create a voltage approximately 2.5 to 3 volts below a positive rail, depending on the zener selected. The rail can vary from 11 to 16…
Part Number: DRV2605L-Q1 Tool/software: Hi team,
It's the 1st time for my customer to design a display which can automatically rotate the content displayed when the screen is rotated. They are evaluating DRV2605L-Q1, but they don't have much idea…
Part Number: LM4040-N-Q1 Tool/software: what is the operating temperature range for the LM4040A41IDBZR. On Mouser, it states -40 to 125 C, but the datasheet does not match that information. Also the datasheet says there is an extended temp range of …
Hello,
I hope somebody answer my querstion.
I completed the TCAN4550 initialization refer to the TCAN demo, but when I called the function
TCAN4x5x_MCAN_ClearInterruptsAll // Resets all MCAN interrupts (does NOT include any SPIERR interrupts).
then I…
Part Number: TDA4AP-Q1
Tool/software:
Hello, is it possible to swap the P/N pins for SERDES2_TX2 / SERDES2_RX2 (pins AR21, AR20 / AU20, AU21) by register setting? We're using this port for SGMII/QSGMII SGMII interface 1.
Thanks for your answer in advance…
Part Number: CDCE6214-Q1 Tool/software: Dear Madam or Sir,
I am planning to use the CDCE6214-Q1.
I do not plan to use the secondary reference clock inputs: SECREF_P/N.
Can I leave these pins unconnected and floating, or should I bias/connect them to…
Hi Tsuji-san
What is the condition difference between below two picture? Is it only the temperature difference with 25C and 80C? It seems quite larger than our results. And the low frequency THD also increased a lot, which indicated the noise becomes…
Part Number: LM4050-N-Q1
Hi Expert,
My customer is doing the FuSa analysis for their system. LM4050 is used in this project. Can you help fill the component type to the excel for LM4050 based on SN29500?
I saw there have SN29500 category in FuSa FIT…
Hi Mingkang,
After clarification with back end team the Reverse breakdown voltage change with operating current change (ΔVR/ΔIR) does need to be taken into account in steady state conditions. The reasoning for describing the load regulation…