Part Number: LMV342 Other Parts Discussed in Thread: LMC6482 , LMC6492 Hi,
I am designing a precision rectifier circuit for one of my design. Here the input is from current sense transformer and this using differential amplifier it will be converted…
Part Number: LMV342 Hello,
Our customer use LMV342 Spice model simulation, and it would appear INTERNAL ERROR when select the temperature(sweep):
INTERNAL ERROR -- Divide by Zero in device X_U1.XU2.D1, Divide
ABORTING SIMULATION
Below is the simulation…
Part Number: LMV342 Hi,
There is oscillation issue in LMV342.
Could you let me know why oscillation is occurred?
Below is the circuit.
AVDD is 3.3V
Vref_L is 0.825V
I'm not sure what R70 and R98 is for.
But when R70 is 240kOhm, U9A output…
Part Number: LMV342 Other Parts Discussed in Thread: TLV9002 , Hi team,
Please let me ask you a basic question. Does LM342 incorporate an internal input low-pass filter that reduces the amplifier response to EMI in the first place?
Sincerely, Tsuyoshi…
Hi Tsuyoshi,
Please use the model available at: http://www.ti.com/product/LMV342/toolssoftware . This is the latest updated macro model. The bandwidth of LMV342 is 1MHz, and the model is limited to this bandwidth that's why there is a shoot up in phase…
Other Parts Discussed in Thread: TINA-TI , LMV342 Hi,
I simulated the LMV342 circuit on TINA-TI.
As result, the phase margin of the circuit is about 9.62°.
Could you confirm it whether it is correct ?
3603.LMV342.TSC
Part Number: LMV342 Other Parts Discussed in Thread: TINA-TI , TLV342 Tool/software: TINA-TI or Spice Models Dear all,
Could you teach me the reason why the TINA-TI results is different from the actual value?
When I input 5V, the output voltage…
Other Parts Discussed in Thread: LMV342 , TINA-TI , LMV824-N Hi,
Oscillation is doubted on the my customer's circuit used the LMV342.
So we would like to confirm operation with the my customer's circuit by TINA-TI.
Can we look oscillation of the…