Other Parts Discussed in Thread: LMV342 Hello,
Could you please kindly let me know the meaning the typical value of Common-mode input voltage range LMV342 ?
For example, V+=5V, GND=0V,
VICR(min)=0V
VICR(typ)= - 0.2V to 4.2V
VICR(max) = 4.0V
Why is this…
Other Parts Discussed in Thread: LMV342 , TLV342
Our customer trying to design an sensing circuit with LMV342 as below.
They want to know the output impedance of this circuit and LMV342 itself.
I think the the output impedance of this circuit is 100Ohm…
Part Number: LMV358 Other Parts Discussed in Thread: LMV342 , TLV9002 , TLV9052 Hi,
LMV358 is under evaluation instead of LMV342.
But due to opamp noise, test results is worse than LMV342.
In the table of datasheet, PSRR, CMRR of LMV358 is better than LMV342…
Other Parts Discussed in Thread: LMV342 Hi,
I have two questions about the graph(Figure-24) in the LMV342 data sheet.
Could you please see the following question?
Could you please teach me? Thanks in advance,
Toshiya
Part Number: LMV341-Q1 Other Parts Discussed in Thread: TINA-TI , LM341 Tool/software: TINA-TI or Spice Models Hi TI team
We have got the request for updated LMV34x-Q1 Spice model for short mode simulation for their failure analysis.
- Does current LMV342…
Yamamoto-san,
We do not have a PSpice model for the -Q1 device in the product folder, however, we do have a TINA-TI model for the LMV342 device (dual version of the LMV341) built into TINA-TI.
Here is the .lib file that TINA-TI uses:
LMV342.lib
You can…
Part Number: MSP430F5310 Other Parts Discussed in Thread: LMV342 , INA168 I'm not sure this is the right forum for this, but I'll start here and see where it goes.
I'm attempting to measure the current on a 48-VDC bus. I have a 50-mΩ high-side…
Gerry,
That was a horrible model. I couldn't even get it to make sense for DC analysis.
I made some edits and used LMV342 model instead. It is not a match, but it is much closer.
RC4580 has less output and input voltage range.
OPA2677 - (TLV342).…
Part Number: LMV341-Q1 Other Parts Discussed in Thread: TINA-TI Hi team,
Do you have "settling time" spec? If no, could you tell me how to calculate or estimate it from datasheet spec and external Cload value? I found that TLV9061S-Q1 has this spec but…