Part Number: LMV393 Hello guys,
One of my customers would like to get LMV393 output rising time/falling time(Tr/Tf?) data to use for their new products.
Could you please tell me those data if you have?
Your reply would be much appreciated.
…
Other Parts Discussed in Thread: LMV393 , TLV1702 , TLC352 , TLC372 , LM393 The output of the LMV393 is open collector, but the datasheet recommends that the output voltage be Vcc + 0.3V Max.
I am looking to pull up the output to 12V. Can I do that…
Part Number: LMV393-Q1 Hello team,
My customer considering using LMV393-Q1 in the automotive application. So this team would like to know about the VICR( Common-mode input voltage range) spec at VCC=5V and full temperature range(-40C ~ 125C). Because…
Other Parts Discussed in Thread: LM393 Hi Jian
I'm using the alternative part LM393 and I'm having a similar problem with the switching functionality.
even when the VIN is less by 300mV than Vref the comparator is switching output state.
Here is…
Part Number: LM393 Other Parts Discussed in Thread: LMV393 Hi everybody,
I was using a LM393D as window detector in one of my design. When the voltage is between 1 and 2.8V, my output is 3.3V and when the input voltage is outside of these values,…
Other Parts Discussed in Thread: LMV393 Hi,
About VCIR of LMV393, please let questions.
The LMV393 use with Vcc=+5V. From the data sheet(SLCS136T), VCIR (Common-mode input voltage range) is specified in the -0.1V to +4.2V.
To us IN- (4pin) terminal…
Other Parts Discussed in Thread: LMV393 , LM393 , LMV358 Greetings,
We have at least a couple LMV393 comparators on a prototype design where they appear damaged (at different times). We've chalked up the first to "maybe it got zapped" but a second time…
Paul;
There is precious little useful information in the 29 page data sheet. The author must have been getting paid by the page. Without some discussion of the topology or even application or test circuits, a user is left in the dark about its behavior…