Hi Tsuji-san
What is the condition difference between below two picture? Is it only the temperature difference with 25C and 80C? It seems quite larger than our results. And the low frequency THD also increased a lot, which indicated the noise becomes…
Hi Mingkang,
After clarification with back end team the Reverse breakdown voltage change with operating current change (ΔVR/ΔIR) does need to be taken into account in steady state conditions. The reasoning for describing the load regulation…
Part Number: LM4050-N-Q1 Hi team,
Could you pls help share below Ir=1mA is spec at what temperature range? Datasheet has list 25C and full temp range spec for Ir=100uA, but didnt specify it clearly for Ir=10mA/1mA
Thank you
Scarlett
Part Number: LMV358-N-Q1 Hello,
I am looking for CDM value of LMV358-N-Q1, datasheet is not showing the value, I am not sure if TI conducted CDM test for this device or it is just missed to print? Could someone please help on this urgently.
Thank you!
Part Number: TAS6424E-Q1 Other Parts Discussed in Thread: TAS6424 Hi TI Team
May I ask how to calculate the TAS6424 or TAS6584 for the THD+N or THD algorithm?
Part Number: TAS2505-Q1 Other Parts Discussed in Thread: TAS2505 Hi Expert,
My customer Bosch is using TAS2505-q1 for quite a long time. We are setting bench to test the THD+N EVM on analog input mode and digital input mode.
Analog Input
I do the test…
Part Number: TLV1822-Q1 Other Parts Discussed in Thread: TLV1822 Hi team,
I am just studying TLV1822 (Open Drain output type comparator)
I have found that if Vin+ >> Vin- , then Vout should be high. it means internal fet should be P Type FET or PNP Transistor…