Part Number: LMV841-Q1 Dear expert, We will be using the LMV841-Q1 IC for our project but we need below parameters:
Failure Mode Distribution
Pin FMEA
Can you provide parameters above?
Your help would be appreciated. Best regards, tatsuya yanagida
Part Number: LMV841-Q1 Other Parts Discussed in Thread: OPA388-Q1 , LMV842-Q1 , Dear expert, We will be using the "LMV842QMA/NOPB","LMV841QMG/NOPB" IC for our project but we need below parameters:
Failure Mode Distribution
Pin FMEA
…
Part Number: LMV841 Hi,
do we have any information on the size of the parasitic caps @ V+ and V- ?
I think it might be even better if we have any kind of load characterisitcs like on the parasitic L and C for these PIN's.
Looking forward to your…
Part Number: LMV841 Other Parts Discussed in Thread: LMV844 , OPA2171 , , LMV842 , TINA-TI , OPA4171 For OPA2171 you don't only provide a figure for max allowed C_LOAD and recommend R_ISO, you also provide a graph of R_ISO vs C_LOAD for phase margins of 45…
Part Number: LMV841
Hello,
The LMV84x datasheet was revised at Oct/2017. I have the question about this revision change.
(1) Phase Marin and Overshoot In the EC table , the phase margin is not difference between Revision I and Revision H.Both specifications…
Hello Carolina,
Yes, I also think that both TLV172 and OPA172 are fit for our application.
About LMV641/LMV841/LPV411, theirs slew rate is too low.
For example, see waveform of the LMV641 TINA simulation:
And what about the OPA992 ? It features too high…
Hi Adam,
I believe the SC70 listing on the first page of the OPA376-Q1 datasheet is a typo that was carried over from the non-automotive OPA376 datasheet. As you found in the package option addendum, we only offer the OPA376- Q1 in the SOT-23 package.
…
Other Parts Discussed in Thread: LMV841 Hi,
I consider LMV841 circuit. Regarding Absolute Maximum Ratings, should LMV841 restrict both VIN differential(±300mV) and Input current(10mA) ? or, all we have only to obey either VIN differential or Input current…
Part Number: LMC6762 Other Parts Discussed in Thread: LM339 , , LMV841 Hello Team,
Customer is asking if there is a negative input voltage vs. Input current curve as attached shown. and is there similar application node available?
LM339 is a Bipolar process…
Other Parts Discussed in Thread: LMV841 , LMV844 I am using the LMV841 (actually LMV844 quad version of LMV841) in unity gain application and I want to know if 10K in series with 4.7uF at the output would oscillate or cause some other unexpected behavior…