Part Number: LMV881 Hello Support team,
Can you clarify if these two LMV881LEE/NOPB labels are the same?
We have two kinds of top mark of 19C and 15E.
Thanks!
Best Regards, Dave
Part Number: LMV881 Hello TI experts,
I want to know about the shutdown function of LMV881.
on page 13in the datasheet, I can see the description as below ;
---
To conserve battery life in portable applications, the LMV881 can be disabled when the shutdown…
Part Number: LMV881 Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models Hello,
I am getting "Element type mismatch" error when trying to simulate LMV881 driving capacitive load.
Simulation circuit works with other…
Part Number: LMV881 Hi,
Page 14 of the datasheet (see table under Figure 29) shows that as the capacitive load increases, the isolation resistor is decreasing - is this correct and how is this calculated?
Thanks,
Chuchen
Part Number: LMV881 Other Parts Discussed in Thread: LM7705
When the Voltage at the positive Input (pin 1) is about 0 to 2 Millivolts, the output (pin 4) is about 72 mV.
The voltage on the output has an offset, that seems greater than what one…
Other Parts Discussed in Thread: LMV861 , LMV881 Hi
We are about to replace AD823 with TI product.
Additionally, we want to the following requirement.
- Input capacitance > 20pF
-Input resistance > 10Mohm
-Small package (smaller than 1.6mm x 2.9mm…
Other Parts Discussed in Thread: LMV881 , LMV861 , LM7321 Hi,
Regarding Output Voltage Swing vs Load Current for LMV881, the datasheet page 9 and figure10, what is voltage for V- ?
In addition, customer would like to use the devices that have a low drop…
Hello,
I'm writing about figure 11 in the datasheet.
The values on the y-axis don't seem right. Is this a publishing error? If so, would you be able to post a corrected graph?
Don
Other Parts Discussed in Thread: LMV881 Hej,
how large is the time between rise/fall of standby-pin of LMV881 and output shortend/released to/from ground? Unfortunatly I could not find this value within the datasheet.