Part Number: LMX2592 Hi,
The LMX2592 EVB board use 0603 components for Loop Filter. Can I use 0402 components to save PCB space? Is there a disadvantage to use 0402 Components?
Thank you in advance. Best Regards,
Tim
Part Number: LMX2592 Hi Experts,
Good day! I have posted this inquiry to confirm our conclusion with our customer.
We are using LMX2592 as an LO in our product. In the low-temperature halt test (-50°C ambient temperature, board temperature is around…
Part Number: LMX2592LMX2592_20MHz.zip
Dear Sirs,
I am having trouble getting stable PLL operation using the LMX2592.
The following are the parameters:
reference frequency: 10MHz
Phase detector frequency: 20MHz
VCO frequency: 6.834682GHz
Integer…
Part Number: LMX2592 When selecting the "Default Configuration" menu item are the register values that are loaded supposed to be recommended values as a starting point, or are they supposed to match what the datasheet indicates as default values? We are…
Part Number: LMX2592 Hello E2E,
Please let me know about the Revision History contents. At the new revision, this device has many changed and added points for register.
I understand that these changes are different depending on when the device was purchased…
Part Number: LMX2592 Hi Team,
Can you help clarify the question below?:
The datasheet states that the output of LMX2592 can be muted by setting OUTA_PD or the other channel as below. If channel A is muted by sending a power down command to its buffer…
Part Number: LMX2592 Other Parts Discussed in Thread: LMX2594 , , LMX2582
Team,
Can you please help with the below questions:
LMX2594. We would like to consider to use LMX2592: https://www.ti.com/assets/js/compareParts/compare.html?familyId=1325&parts=LMX2592…
Part Number: LMX2592 Hi Team,
I have two questions.
1.VTUNE_ADJ
Customer is using 6.5GHz or higher and had the setting set to '0'.
Does this cause any problems?
2.CP_ICOARSE
The datasheet recommends setting it to '0' or '2', but they are set…
Part Number: LMX2592EVM Other Parts Discussed in Thread: LMX2592 Hi Team,
I'm using LMX2592 for a fast VCO frequency sweep. I read from the data sheet and find the fastest speed is about 33us for a new frequency. But I cannot find related support…