Part Number: LMX8410L Hi team
Customer has questions about the CE (pin1) port function of the LMX8410L. Could you support?
Q1. If CE port is enabled, will the register information set by SPI be retained?
Q2. If CE port is enabled, will all RF functions…
Part Number: LMX8410L Hello,
in a very narrowband application working at RF 10 GHz, I would like to downconvert a signal having a relevant content at very low baseband frequencies (100 Hz to 500 kHz) . Unfortunately I was not able to find in the data…
Part Number: LMX8410L Hi team,
Customer wants to use LMX8410L and they want to achieve below.
RF input frequency = LO input frequency, then, they want to get IF output frequency = DC.
Now they have questions about mixing spurs that is explained on 3…
Part Number: LMX8410L Hi Expert,
We would like to know how much RF power we should back-off to keep EVM performance while the RF input power level is maximum.
May we have the EVM versus RF input level test result for LMX8410L?
Thanks a lot.
Derek
Part Number: LMX8410L Other Parts Discussed in Thread: , LMX2594 Hi,
I'm using the LMX8410L's LO as output. I have the LMX8410LEVM board. I put 50ohm resistors on the board as LO pull-up. According to the datasheet Fig 44, shall I expect 2dBm output…
Part Number: LMX8410L Hi team,
Customer guess that Integrated LO can affect the performance of I/Q demodulator and they want to understand how much the LO can affect the the performance of I/Q demodulator quantitatively.
Are there any app notes for this…
Part Number: LMX8410L Other Parts Discussed in Thread: LMX2594 Dear team
There is a good news that we design in LMX8410 in customer's new project. Customer have some question about thermal, could you help to recommend?
1.What is the chips default status…
Part Number: LMX8410L When I use the DCOC function of LMX8410l, I find that it takes 10ms to achieve the result I want. I want to shorten the time to less than 1ms, what should I do? Thank you!
Part Number: LMX8410L Other Parts Discussed in Thread: LMX2594 , PLLATINUMSIM-SW Dear team
There is a good news that we design in LMX8410LRGZ in customer's new project.
Could you help to review the schematic?
thanks
denny
Hi Dean,
Thanks for answers, it is very helpful.
As mention above, LMX8410L have a large output Vpp, how to attenuator it for our ADC input? our ADC input can handle Vpp 0.8V only.
Thank you.