Part Number: LMX8410L Other Parts Discussed in Thread: TRF370417 , I have a ADC/DAC that generates Differential IQ with > 1GHz instantaneous bandwidth (4 MSPS). I am looking at LMX8410L and TRF370417 to modulate and de-modulate basband signal to 4GHz IF…
Part Number: LMX8410L Hi sir,
I have some inquiries on this devices.
Can you clarify these queries?
1.Can the frequency synthesizer of LMX8410L produce frequency modulation signal? 2.If I use the software to set the VCO frequency, do I need to set it again…
Chen,
Before the LMX8410L was released, there were some earlier versions of this device with very similar pinout. On the earlier version of this device, Pin 34 was an ATP test point. I think the legacy of supporting this is why this pin was not grounded…
Part Number: TRF370417 Other Parts Discussed in Thread: LMX8410L , 1) Does TI have a part with > 1GHz bandwidth than TRF370417 ? I am pairing it with LMX8410L
2) Is there a reference design showing both TRF370417 (or an alternative) and LMX8410L and a…
Part Number: LMX8410L Hi Team,
Can the integrated synthesizer of the LMX8410L generate Chirp (LFM) signal ?
If it can - can you please give some information of any df/dt or BW limitations ?
Regards,
Nir.
Part Number: LMX8410L Hi team,
My customer has the following questions about lmx8410, and I am not familiar with RF. Please help me. Thank you in advance.
Use two lmx8410 evaluation boards.
OSCin 50MHz
LO 4860MHz
RFin 4800MHz
IFout 60MHz
SYNC is 10MHz…
Part Number: LMX8410L I have a reg load list of values from the eval software but notice that registers 120 and 106 are not included in the listing. Are these essential or do they have correct default values already in them?
The data sheet dated nov 2018…
Part Number: LMX8410L From 7.4.1.1
Although the majority of devices have a VCO range of 7.5 to 15 GHz, this is NOT ensured. In reality, the VCO is tested for sure to cover 7.7 to 15 GHz. In the range of 7.5 to 7.7 GHz and 15 to 15.4 GHz, the VCO will…