Other Parts Discussed in Thread: LMZ10501 Hello
I simulate LMZ10501 by WEBENCH.
Tj is written in operating values, but it isn't written about having air or not.
Could you please let me know about having air or not?
Best regards,
Yokota
Hello,
Have you been able to measure the waveforms/ voltages on the nodes as suggested by Yang before? We want to make sure the parts are dead before we proceed ahead. Have you measured for any shorts on the board after the output died?
Regards, …
Other Parts Discussed in Thread: LMZ10501 , LMZ31503 Hi
My customer estimates the value of output decoupling capacitor.
Therefore he needs the parasitic inductance and resistance of the Vout and PGND terminal of LMZ10501.
Could you tell me the values…
Hi,
any news for me?
Replacing the damaged LMZ10501 on one of the damaged electronics, solved the issue there, the board is working again as expected. So it really looks like something is damaging the LMZ10501 during power-on. Our customer uses various…
Other Parts Discussed in Thread: LMZ10500 , LMZ20501 , LMZ10501 , TINA-TI Dear Community,
we have a great base of models and knowledge in LTSPICE and currently try to run the LMZ10500, LMZ10501, LMZ20501 pspice models in LTSPICE.
Always the same…
Hi Denislav,
First of all thank you for your detailed answer!
Second, What did you mean when you wrote "i f you don't need more than 1A of output current, you can also achieve this with a single LMZ10501 module", are you implying that if I use two…
Other Parts Discussed in Thread: LMZ10501 Hi,
How can I margin the LMZ10501 output voltage (+/-5%) with a standard margining DAC (e.g. 0.6V to 1.2V)?
Thanks,
Noam
Other Parts Discussed in Thread: LMZ10501 Hi,
I want to implement current sharing from two LMZ10501 Nano Modules to get at least 1.8A at the output.
Is there any reference for something like that?
Thanks,
Michael
Other Parts Discussed in Thread: LMZ10501 On the LMZ10501 datasheet page 2.
The EN pin is internally pulled up to VIN, if left floating the chip is always on.
This may be a problem on our application.
Do you have an equivalent part that has no pull…
The name of an ap note for the LMz14203 is.
Inverting Application for the LMZ14203 SIMPLE SWITCHER ...
The link for that ap-note is
www.ti.com /lit/an/snva425a/snva425a.pdf