Other Parts Discussed in Thread: LMZ10504 Hi,
I have a question about internal connection of the LMZ10504.
Is exposed pad connected to ground terminal internally? (My question is connection between exposed pad and ground terminal inside of thie device…
Hi,
So from my understanding on page 13 of the datasheet, when using this part you want the EN input to be either based off the input voltage or output voltage. There is no reason to have the EN pin turned on before the input to the IC.
My question…
Other Parts Discussed in Thread: LMZ10504 Hello,
We are using the LMZ10504 module in application where the Output load capacitance can vary from 22uF to 220uF.
We need to ensure the stability of the module other all the output capacitance range…
Hi Giuseppe,
The LMZ10504 runs at 1 MHz switching frequency. The output ripple should be small. I've run a Webench design on the LMZ10504 and the output voltage peak-2-peak ripple is 8mV with one 220uF 15mOhm output capacitor. If further reduction is…
Other Parts Discussed in Thread: LM3150 Hi,
I'd like to ask about the need of external ripple injection circuit for LM3150.
According to the attached PDF file page 14,
It saids that we need the external ripple injection circuit when the output voltage…