Other Parts Discussed in Thread: LMZ13610 sir,
i would like to use LMZ13610 to derive +3.3V for my circuits from -24V input, can i use this LMZ13610, if yes please suggest circuitary for the same.if not please suggest an alternate for the same.
with r…
Other Parts Discussed in Thread: LMZ13610 Hi,
I need to know what happens if the component LMZ13610 receive a voltage greater than 36V (maximum voltage input as data sheet)?
tanks
Eng. Antonio Valquendis
Other Parts Discussed in Thread: LMZ13610 Hello,
I have to implement a DC/DC converter that inputs 8V-19V, and outputs 5V@10A. The LMZ13610 at first glance fits, but there are doc confusion : the data sheet gives an input range of 7..36V for 5V output…
Hi John,
Thanks for your quick support.
We want the regulator which is having internal inductor, i meant to say integrated inductor Like LMZ13610.
Can u please suggest the similar simpler switcher power module.
Thanks & regards,
Divya
Hi Mike,
I want one more clarification regarding VA supply pin.
Now we have planned to provide 5V supply as input( because analog signals source voltage is 5V), which is generating from LMZ13610 regulator In In layout side we are planing place these…
Other Parts Discussed in Thread: LMZ13610DEMO , LMZ13610 I plan to use the LMZ13610DEMO board to create a constant current supply by tinkering with the feedback from an external current sense resistor. When the load is removed, the LMZ13610 will have no…
Other Parts Discussed in Thread: LMZ23610 , LMZ13610 Hi, I intend to use the LMZ13610 or LMZ23610 in a 24 V vehicle and I need to have my product compliant with ISO-16750-2[24 V system]. So I m looking for a low cost solution that allows the power supply…
Thank you Akshay
Actually I need more output currents and I was looking for a high output current converter. The one that you mentioned seems to be good for wide input voltage range but not good enough fot output current
Anyway what I did was using two…