Part Number: LMZ14201 Dear TI,
Are there any MTTF or FIT numbers for LMZ14201 switching power supply? They are not shown on TI reliability page.
Thank you,
Dmitri Chtchvyrkov
Part Number: LMZ14201 Tool/software: WEBENCH® Design Tools Hi,
i needed a 12V to -12V converter with 0.5A, got this design:
i have 2 things i dont understand in this design and will be happy if you could explain them:
1. The Cbyp capacitor see 24V and…
Part Number: LMZ14201 Other Parts Discussed in Thread: LM3880 I have a customer in the sequencer Forum using the LMZ14201 with a LM3880 sequencer.
He has experienced a damaged sequencer when connecting the FLAG1 output of the LM3880 to the LMZ14201 Enable…
Part Number: LMZ14201 Other Parts Discussed in Thread: LMZ14203 The particular application I intend to use the LMZ14201 power module for requires it to operate in the presence of the a large electromagnetic field. Is there any documentation for this product…
Part Number: LMZ14201 Other Parts Discussed in Thread: LMZ14202 , , LM3880 , LMZ14203
Hello
I have a concern I try to command a LMZ14201 and LMZ14202 , following the proposed schematic with the resistor divider
( LM3880 is set with 100 K resistor ballast…
Part Number: LM3880 Other Parts Discussed in Thread: LMZ14202 , , LMZ14201 , LMZ14203
Hello
Thanks to Brad for reference LMZ mistake
I have another concern I try to command a LMZ14201 and LMZ14202 , following the proposed schematic with the resistor di…
Part Number: LMZ14201 Other Parts Discussed in Thread: LM3880 Hello
Great to have close all the threads without to have wait a solution
so my situation is still NOT SOLVED
I have test with a buffer transistor ( NPN 4401 ) wit several resistor value…