Part Number: LMZ14201H Other Parts Discussed in Thread: LMZ14201 Tool/software: WEBENCH® Design Tools Using WEBENCH POWER DESIGNER created a design using Part # LMZ14201H.
Dc input 12-13V , Output -5V , Output current 0.5A.
My question is Cout capactiance…
Part Number: LMZ14201H Hi Team,
A customer tried to simulate LMZ14201H with the following specifications, Vin =11V-14V, Vout=10V and Iout=0.5A. However, an error message below appeared in Webench. Is this a bug in Webench or because the difference between…
Part Number: LMZ14201H Other Parts Discussed in Thread: LMZ14203H , , LMZ14201 We use the LMZ1420xH series for many applications.
As already asked in the original thread, we experience EMI problems at 60-70MHz and 200MHz.
We tested different output…
Part Number: LMZ14201H Other Parts Discussed in Thread: LMZM23601 , LMZ34202 , TPA2005D1 , LMZ14201 Can the LMZ14201H be regulated down to 4.2V output ? The input voltage is 12V.
Part Number: LMZ14201H Other Parts Discussed in Thread: LMZ14203H I need to develop a variable output power supply module capable of supplying a 5-24 volt output voltage at 5-1000mA. In experimenting with the LMZ14201H module in the WEBENCH tool, I struggled…
Hi byliu,
Thank you for your feedback. We will take that into consideration for future roadmap device discussions. As of right now the power module's team is primarily focused on creating buck modules.
Regards,
Jimmy
Hello Byliu,
Yes, you can use the LMZ14201H with the Application note. The "H" and the non"H" devices are pin-to-pin compatible.
It is OK to tie EN to VIN.
Cheers,
Denislav
Part Number: LMZ14201H Hello,
We have a customer asking about the datasheet definition for the ECO Plan for this device.
It shows "RoHS (In Work) & Green (In Work)". The date on the Package Option Addendum is 27-Apr-2017. The customer purchased this…
Part Number: LMZ14201H Hi
this power module's output voltage is 5V. and this 5V output is parallel with USB power to facility debug working without powering on the whole board.
question is that: is it safe for this power module if its output has 5V…
Part Number: LMZ14201H Hello,
I am using the LMZ1420XH series in many projects as a preliminary DC-DC converter for the first stage of the circuit, continued in the second stage by linear LED drivers.
Recently some EMI tests failed at unexpected high…