Part Number: LMZ14202 Other Parts Discussed in Thread: PSPICE-FOR-TI Hi Team,
I'm trying to simulate LMZ14202 part using TINA simulator for 24V to 5V conversion as shown in the below
I tired to simulate but getting below error
Request to assist…
Part Number: LMZ14202 (Assigned) customer is using LMZ14202 and would like to measure stability over temperature of their particular design.
They have noted the following statements in the datasheet:
“The control architecture for this part is a "constant…
Part Number: LMZ14202 Hi Team,
I designed a circuit for following conditions
Input voltage = DC24V
Output voltage = DC 3.3 V
Q1: supplying input voltage
24V → 15 V (continued for 30 milliseconds) → 24 V
If an instantaneous power supply change…
Part Number: LMZ14202 Hi Team,
I designed a circuit for following conditions
Input voltage = DC24V
Output voltage = DC 3.3 V
Q1: supplying input voltage
24V → 15 V (continued for 30 milliseconds) → 24 V
If an instantaneous power supply change…
Part Number: LMZ14202 Other Parts Discussed in Thread: LMP8646 , LMZ14201
We have a situation where we are seeing approximately 0.9V on the output of the LMZ14202 when the EN pin is low (close to 0V) and the input supply is ~ 24V.
The load is a passive…
Part Number: LMZ14202
Hi all,
I have been simulated this simple switcher using Pspice for TI. As its datasheet states, the switching frequency can be calculated using a formula.
Anyway, by using a specific value for Ron, the calculated frequency is about…
Part Number: LMZ14202 We use the LMZ14202TZ(E/X)-Adj/NOPB since some years in different applications, but now it is no longer available by distributors like Digikey oder Mouser.
The LMZ14202EXT is available, but what's the difference between these? Only…
Part Number: LMZ14203EXT Hi, Good day. Our customer is looking for the possibility to use the LMZ14203EXTTZ/NOPB in place of LMZ14202TZ-ADJ/NOPB as they are having sourcing issue. They want to confirm if they can do use it without changes to existing board…
Part Number: LMZ14202 Does this LMZ14202TZ voltage regulator has any kind of UL certification or will it affect when applying for CE certification to a product that include this Regulator.