Hello Chris,
Here is some background on the part.
At light load the device enters discontinuous conduction mode. In this mode of operation the switching frequency will decrease with the load going down. As a result of the lower frequency, there…
The LMZ14202H can be used depending on your input voltage.
The current in an inverting design is the input current + the output current.
For example. 24V to -15V at 1 A.
Input current is 1A *15/24 = .625 A
Output current is 1 A
Efficiency is…
Other Parts Discussed in Thread: LM3150 Hi,
I'd like to ask about the need of external ripple injection circuit for LM3150.
According to the attached PDF file page 14,
It saids that we need the external ripple injection circuit when the output voltage…