Part Number: LMZ14203 Tool/software: WEBENCH® Design Tools Hi all, I have some troubles with LMZ14203 DC-DC Step-down converter.
The Datasheet is declaring 8mVpp of ripple, while in reality I am measuring 340mV over my board.
This is the WEBENCH proposal…
Part Number: LMZ14203 I am reading AN-2024 and it states that "Gerber and CAD files can be download from the LMZ14203 product folder" but they are not there. Where can they be located?
Part Number: LMZ14203 Hello,
I have a prototype board based on the layout and bill of materials of the eval board. The output is set to 13.2v and the input is from a full wave rectifier coming from a transformer. I was doing load step testing and I was…
Part Number: LMZ14203 I have a LMZ14203 with a circuit straight out of the data sheet. The two differences are that my Rfb resistors are of higher value (12.3k/2.2k for 5.15V output), and the Ren divider is of lower value (10k / 1.5k for 8V). Local input…
Other Parts Discussed in Thread: LMZ14203 , LMZ14203H Hello,
Could you please clarify which is the true maximum output voltage of LMZ14203?
In the datasheet there are numerous references to higher output voltages of up to 30 V.
In the Webench simulation…
Part Number: LMZ14203H Other Parts Discussed in Thread: LMZ14203 , Even if a short occurs in the LMZ14203HTZ output power, the Protection function does not operate.
Even if you forcibly short pins 1 and 2 of J19, the protection function does not work.
…
Other Parts Discussed in Thread: LMZ14203 Hi,
To get a lower output ripple on the LMZ14203, we used the following circuit. (See below)
Now the opposite happens, going from a ripple of 20-30mVpp to a ripple of 100mVpp+
L1= Coilcraft - MSS6132-682MLC
6.8uH…
Other Parts Discussed in Thread: LMZ14203 Dear all,
I would like to know where to find the Orcad/Cadence files for the EVAL board for this device. I have read in the Application note "AN-2024 - LMZ1420x/LMZ1200x Evaluation Board", on page 8 that "Gerber…