Hello Joshua,
There are several limitations for going beyond 15V. There is an internal regulator deriving the VCC bias from VOUT once the part is up and running. That has a maximum input of 16V. Also, with larger output voltages the inductor ripple current…
Part Number: TPS54240 Other Parts Discussed in Thread: LMZ14203H , LMZM33603 , LMZM33604 Hi team, I am looking for a fully integrated buck converter having characteristics close to the TPS54240: - Large Voltage input : <9 and >24V - Low Iq <1mA (enabled…
Part Number: LMZ14203HEVAL Other Parts Discussed in Thread: LMZ14203H , Hello,
My client wants to use the LMZ14203H component in his design, At the moment he plans to do rapid development and looking to stitching the evaluation board (as is) in his design…
Part Number: LMZ22010 Other Parts Discussed in Thread: TPSM84A22 , TPSM84A21 , LM317 , LMZ14203H , PTN78020W Is this LMZ22010 module a fair candidate for a programmable supply via pot, I2C pot, DAC, etc.?
Other Parts Discussed in Thread: LMZ23610 , LMZ14203H , LMZ14203 The output voltage range0.6-6V.Now my output voltage is 8V.there is no problem.Also, The input voltage range is 6-36V,why the output voltage is so low.
I would like to know the risk when I…
Hello Damien,
first I can recommend for your application the LMZ14203H for your desired output voltage of 13.2V. The LMZ14203 is only recommended for output voltages up to 5V.
Second, some more information could help to solve the issue:
- Please provide…
Other Parts Discussed in Thread: LMZ14203 , LMZ14203H Hello,
Could you please clarify which is the true maximum output voltage of LMZ14203?
In the datasheet there are numerous references to higher output voltages of up to 30 V.
In the Webench simulation…
Other Parts Discussed in Thread: LMZ13608 , LMZ14203H Dear all,
I want to set output voltage of LMZ13608 to 7V .
The load current is less than 2A.
Can I set to that?
Hi Hendrik,
The higher ripple and bump in regulation is expected at light load. When the load is low and the part is in DCM mode of operation, the switching frequency will decrease to minimize the switching losses and maximize conversion efficiency. The…
Other Parts Discussed in Thread: LMZ21701 , LMZ14201H , LMZ14203H , LMZ14203 Can I use the TI LMZ14201H type SIMPLE SWITCHER MODULE (or, more generally, all of the SIMPLE SWITCHER MODULES including the high-density Nano Modules --e.g. LMZ21701) in an inverting…