Part Number: LMZ20502 Other Parts Discussed in Thread: TPS82084 Dears,
I am now trying to select a power module. I find both LMZ20502 VS TPS82084 are suitable to my case.
They have similar function. Could you please tell the different between each others…
Part Number: LMZ20502 Hello TI Team,
Do you tell me what process of gold deposit is used (electrolytic or chemical) and what thickness of gold is deposited on the terminations of this component knowing that they are finished NiAu and not NiAuPd.
Thank…
Part Number: LMZ20502 Other Parts Discussed in Thread: LMZM33606 Hi , I was wondering if the above parts can be paralleled to provide up to 4A of current?
Thanks
Paul
Part Number: LMZ20502 Other Parts Discussed in Thread: TPS82130 , LMZ10503 , LMZ30604 , LMZ30606 We are using the LMZ20502SILT and on 4 of our boards the part "goes bad" after a few power cycles. The failure mode is a very low ohm reading to ground at the…
Part Number: LMZ20502 We are using LMZ20502SILT to convert from 3.7V to 3.3V.
As per data sheet it is recommended to use RFBB = 53.2 kΩ and RFBT = 237 kΩ.
We cannot find 53.2KΩ of desired size we need (Size required: 0402).
So we need to…
Other Parts Discussed in Thread: LMZ21701 , LMZ20502 Both parts are listed as EMI tested in the TI product selector. However EMI test data is limited or non-existent in datasheets:
1) LMZ21701: There are 2 EMI graphs (Fig 10 and 11) at Vin = 12V, Vout …
Other Parts Discussed in Thread: LMZ20502 Hi,
I have a board where LMZ20502 is fed with 5 volt input, and should give 1.8 volts output.
The enable pin is controlled by an FPGA, which floats it's output during FPGA configuration download. The enable pin…
Other Parts Discussed in Thread: LMZ20502 , LMZ20501 , LMZ21700 Does LMZ20502 start into Pre-Biased loads? If I switch quickly power on/off and output capacitors are still charged does it sink current or is there other problems (mayby broken circuit)?
…