Part Number: LMZ21700 Product number: LMZ21700SILT
Please provide environmental data for LMZ21700SILT. It's not even listed on TI-Web, which is very troubling. Die(Si), Substrate, Plating, Chip-C, Chip-R, Chip-L All MCDs must be listed.
thank you…
Part Number: LMZ21700 Hi Expert,
Can You check and confirm below top marking of the device and label?
MPN : LMZ21700SILR
device marking : 25Q KRQ
Label : Item 23
Image attach for your reference.
Label item number should match with the unit…
Part Number: LMZ21700 Hi :
about lmz21700, I want to know if the PG must be used ?if not , just float it ?
hope for your reply.
Thanks and best regards
Kim
Part Number: LMZ21700 Hi Experts ,
Can you check and confirm below markings of label and unit markings are consistent with the TI requirements ?
Really Label item no should match with the unit markings of the part .
Looking for your support on validating…
Part Number: LMZ21700 Looking to have a socket created to bench test a LMZ21700. What is the min/max dimensions for label A? For clarification, is 0.08 the measurement between the copper pad and the base of the PCB?
Thank you.
Part Number: LMZ21700 Other Parts Discussed in Thread: TPS82150 We are designing new DCDC. now we are considering LMZ21700 or TPS82150 for new design. Both meet our design requirement. we only need 0.2A for 5Vout
from TIonine store TPS82150 is slightly…
Part Number: LMZ21700 Hi Support,
I have a question regarding LMZ21700's load regulation at light load.
As illustrated in the plot, <10mA, the regulator seems to enter another operating region. From my estimation (I am using 12V to 5V), the PSM…
Part Number: LMZ21700 Hi,
We're designing a product with LMZ21700 . For EMI tests, we shielded the power block with RF shield. Before the power block, we have LC filter, which is BNX026H01L . Should we also use shield for our LC filter for EMI tests…
Part Number: LMZ21700 Hello,
I am using the LMZ21700 with an output at 6V/50mA.
In these conditions, what is the minimum input voltage to ensure proper operations?
Looking to figure 8 and 9 in the datasheet (doc number SNVS872C) does not help, because…