Other Parts Discussed in Thread: LMZ22008 I'm looking to generate -4.25V from +12V using the LMZ22008 simple switcher and having trouble getting it to run. During debug, I have a very light load (100mA) and I'm getting my Vout to look like...
I…
Other Parts Discussed in Thread: LMZ22008 , LMZ12010 Dear Sir/Madam,
I have a PCA that uses 4x LMZ22008 and 1xLMZ12010. A high failure rate has been observed on the LMZ22008 (approx 40%). A low failure rate has been observed on the LMZ12010 (approx…
Hi Grant,
Could you provide sch, layout and BOM for the LMZ22008 with 3.3Vout? Also what is the load level when you hear the audible noise? Was it there with any load or just a narrow range of load?
Thank you,
Yang
Part Number: LMZ22010 Other Parts Discussed in Thread: LMZ22008 , LMZ23610 , LMZ13610 Hi Team,
Is there a recommended part number to P2P replace LMZ22010TZE?
Thank you.
Best Regards
Darren
Part Number: TPSM84824 Other Parts Discussed in Thread: UCC39002 , LMZ31710 , LMZ22008 , Hi,
Will two TPSM84824s be able to use as single 16A output with same circuit using UCC39002 like described the following app note?
https://www.ti.com/lit/an…
Hello Vijay,
Both TPS56121 and LMZ22008 are appropriate for the design. LMZ22008 is easier to use with a higher level of integration.
Best Regards,
Bob Sheehan
Other Parts Discussed in Thread: LMZ22003 , LMZ22008 Hello,
I am working with a design that is migrating from the LMZ22008 to the LMZ22003. The issue is that the LMZ22008 was capable of running at lower frequencies down to 350kHz which made using…
Other Parts Discussed in Thread: LMZ22008 , TPS53318 Dear Sir/Madam,
I am looking at TPS53318 to replace an existing LMZ22008 design.
Previously I have achieved very low output ripple < 20mV pk-pk @ 8A using low ESR polymer capacitors.
Page 7 has…