Part Number: LMZ23605 Hello team,
my customer is looking for more information about the SYNC pin:
- in the "typical application schematic", a resistor is shown, which connects the SYNC pin to ground. Is it necessary to use the resistor, when synchronisation…
We are seeing ~5% fallout with devices internally shorting AFTER reflow soldering. I have profiled the devices on the PWB and component body briefly reached 241C during peak reflow. I also ran several boards with a cooler profile body temp 229C and still…
Other Parts Discussed in Thread: LMZ23605 , LMZ35003 , LMZ14203H , LM43603 Hi, I plan to use LMZ23605 to regulate a 14.4V-12V source down to 11.0V (@1A to 3A loading), Is there any minimum Vin-Vout requirement? I also cannot find the efficiency graph of any…
Just to give a heads-up (1 year later as I forgot to post a reply). Better late than never
1) You were correct about this prediction when both of them have the same voltage setpoint (though not really the same because of component tolerances), and this…
Other Parts Discussed in Thread: LMZ23605 The datasheet of the LMZ23605 stated on page 17:
"Additional bulk capacitance with higher ESR may be required to damp any resonant effects of the input capacitance and parasitic inductance of the incoming supply…
Other Parts Discussed in Thread: LMZ23605 I want to test two LMZ23605 to get positive and negative voltage.
For a first shot, I want to us the eval board. What is the main difference between the eval borad and the demo board?
Is it only the blank pcb or…
Hello Ryuji,
This is an interesting situation. It looks like you are trying to obtain a 0 to 7V output voltage using the DAC adjustment of injecting current in to /(out of) the feedback node.
In general, most step-down regulators will have issues once…
Other Parts Discussed in Thread: LMZ23605 Is the LMZ23605,has UL,VDE etc certification?.
Can I connect it directly to outside power or I need additional filters for compliance with the Safely Labs?
If filters are needed, do you have recommendations?
…