Part Number: LMZ23610
Hi,
The customer's power supply product uses LMZ23610 chip, with an output of 5V/50A. Five chips are used to work in parallel, but a failure phenomenon has occurred and the cause cannot be found. Comparing the chip datasheet…
Part Number: LMZ23610 Other Parts Discussed in Thread: TPSM63610 Hello expert,
Customer would like to have LMZ23610 comparison tale with MPS/LTC. May we know if you could provide the table for us? Thanks a lot!
Best regards,
Ann Lien
Part Number: LMZ23610 Other Parts Discussed in Thread: LMZ31710 , Hello,
I want to use lmz23610tz or lmz31710 to design 12V input and 5V / 8A output. I want to know whether these two chips need to be equipped with heat sink or…
Part Number: LMZ23610 Hi, in my project i have the situation in the attached image about current sharing with 2 LMZ.
Pin Enable are linked together. We want turn on and turn off output of the module controlling enable pin. We see that if connect enable…
Part Number: LMZ23610 Hi,
One of our customer is using LMZ23610 Switcher module with enable.
They want the output only when VIN is greater than 21V.
w.r.t Section 8.2.2.2, 12.7 kΩ for RENB and 42.2 kΩ for RENT resulting in a rising UVLO of 5.51…
Part Number: LMZ23610 Hi Dear,
Can I use LMZ23610 as IBB with input range 9-36V and output will be -5.5V at 9A?
If it is possible can you provide any reference application note?
I have tried using Webench but it says that it is not possible using…
Part Number: LMZ23610 Hello, We have been using LMZ23610TZE/NOPB in our designs for years. The recent manufacturing run for our mobile robot found 10/60 units to have faulty LMZ23610TZE/NOPB.
3/10 failures had LMZ23610TZE/NOPB that would not boot…
Part Number: LMZ23610 Hi
Please help check the attached file. 3858.lmz23610 three models.docx
Please give some suggestion for this problem.
Thanks
Star
Hi Randall,
As John pointed out, the datasheet only specs the LMZ23610 for applications up to 6V. Since the inductor is integrated into the power module, the system has been tested to be stable under the condition that Vout does not exceed 6V. It may…
Part Number: LMZ23610 Hi team:
Efficiency is very low by using the LMZ23610 power module.
Input voltage is 18 V, input current is 1.033 A.
Measured output voltage is 4.863, output current is 2.4A. Efficiency is only 62.8%.
Operated at room temperature…