Part Number: LMZ23610 Hi team:
Efficiency is very low by using the LMZ23610 power module.
Input voltage is 18 V, input current is 1.033 A.
Measured output voltage is 4.863, output current is 2.4A. Efficiency is only 62.8%.
Operated at room temperature…
Part Number: LMZ23610 Hi
Please help check the attached file. 3858.lmz23610 three models.docx
Please give some suggestion for this problem.
Thanks
Star
Part Number: LMZ23610 in page 13 of the app note SNVA538, shows a equation for the input impedance of a buck converter
see image below
is there an explanation how this formula is derived? or
do you know where I can find more information about this equation…
Part Number: LMZ23610 LMZ module seems to work fine with high output current capability.
However, I noticed that this module rated for up to 6VDC output is capable, via the resistor divider network, of much greater output voltages.
Is this is typical…
Part Number: LMZ23610 Hi,
I have a LMZ23610 configuration in negative output mode to generate -6V at 6A maximum from a 12V input.
My question however, is general and concerns the use of the SYNC input. I would like the regulator to start up and generate…
Part Number: LMZ23610 Hi,
I have a follow up question on the sharing aspect of this device. The data sheet states that you can parallel up to 6 devices, however, the evaluation board datasheets does not have a limit (as long as you take in consideration…
Part Number: LMZ23610 Hi,
I am looking into using this device for a project that requires Vin 18-36VDC and VOUT 5VDC@60A, efficiency needs to be above 80%.
I have a couple of questions:
How much is the efficiency of this device changes while is in current…
Dear Akshay,
Could you please pay attention to the outstanding quality issue LMZ2360?
because our customer has got crazy disaster situation now.
I'm looking forward to hearing the comment of yours as soon as possible.
Thanks and best…
Part Number: LMZ23610 Tool/software: WEBENCH® Design Tools hi,
i attached here the next link:
https://webench.ti.com/appinfo/webench/scripts/SDP.cgi?ID=7937D62F4F500AE5
the issue is there, please your help.
thanks,
itzik
Part Number: LMZ23610 Hi,
Could you give me the EN hysteresis source current MAX & MIN value,The Value can't be found in datasheet!
I test my board found that the EN hysteresis source current max value maybe 70uA,
Test Value is En(on…