Hi Rob,
There is no issue with having too much input capacitor. The only problem that i can see is that the upstream supply might hit a current limit because of the inrush current going to the input capacitor of LMZ30602.
Just make sure you have a…
Hi All.
Please tell me the following two points about Adjusting VIN UVLO.
1.One instance of VIN UVLO is given in Table8 of date sheet. Please tell me calculation method of this instance.
2.If there is no error of RUVLO, how much is the variation…
Hi All.
Please tell me the following two points about slow-start time.
1.One instance of SS time is given in Table6 in date sheet. Please tell me calculation method of this instance.
2.If there is no error of CCS, how much is the variation in the…
Hi Rob,
The part should come up for the requirements you've listed. (Making sure that the load grouping is still below 2A)
If you especially want modules, on the Loads entry page, on the right hand side there is a button that says "Show More Options…
Other Parts Discussed in Thread: LMZ31520 , LMZ30602 Hi~
Our customer will use LMZ30602 and LMZ31520.
If see LMZ30602 datasheet(19Page), it mentioned as bolow comment for sequensing
Many of the common power supply sequencing methods can be implemented…
Other Parts Discussed in Thread: LMZ30602 , LMZ31710 Hi All,
Now our customer has evaluated LMZ30602 and LMZ31710, then they found that the absolute maximum rating of VOUT pin is different between these two devices. Specifically it's depend on VIN for…
Other Parts Discussed in Thread: LMZ30602 , LM10010 Hello,
Could you please let me know the value and acuracy of Internal feed back resistor in LMZ30602 VSENSE pin (red circle in below image)?
Since I would like to use LM10010 for adjustment Vout…
Dear specialist
Our customer has a question where should PGND be connect.
They think PGND should be connect at PGND plane reffering Figure19,20 but page21 describes PGND should be connect with AGND at one point.
Which is your recommended?
Please…
Other Parts Discussed in Thread: LMZ30602 Hi,
First of all - I like to thank you for the quick replies!
Just to double check - Can I use LMZ3060 4 layout for LMZ3060 2 or the LMZ3060 6 ?
Thanks,
Noam
Part Number: LMZ30606 Other Parts Discussed in Thread: LMZ30602 , , TPS82085 Hello,
Unfortunately I cannot find anything about pre-biased startup for LMZ30602/4/6. Is this possible for these devices?
If not - what is the maximum voltage allowed at…